1. What is the method for programming the work done in code warrior in t1042?
2. Also, what are the program tools?
ex) xilinx, ise impact
Plz, give me a beginner's guide if you have one.
Please refer to this step by step user guide about CodeWarrior flash programming for Power Architecture.
Please download and install CodeWarrior 10.5.1 from the following link.
https://drive.google.com/file/d/18YIFeSnzZlcE1ZgSNUlTYM955gh9_B56/view?usp=sharing
1. Please configure your target board as hard-coded RCW if no valid RCW on the target board.
2. Please create a bareboard project with SRAM launch configuration selected.
3. Connect to the target board from Run > Debug Configurations.
4. Please execute the flash programming task.
You could use JTAG configuration file to override RCW on the target board.
Please refer to section "8.4 Setting up a remote system to use a JTAG configuration file" in C:\Freescale\CW_PA_v10.5.1\PA\Help\PDF\Targeting_PA_Processors.pdf.