T1042 pin table for creating parts

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

T1042 pin table for creating parts

1,260 Views
akowalczyk
Contributor II

Hello!

We are using a T1042, and found a pin table on this forum to help create the part. However, it looks like the pinout provided has repeated pins based on each peripheral. Is there a version of this pinmux document that does not have the repeating pins for each peripheral, so we can plug into our schematic symbol generator?

 

Thank you for your help!t1042_pinmux.png

Labels (1)
0 Kudos
Reply
3 Replies

1,218 Views
akowalczyk
Contributor II

Hi Hector,

Thank you for the response. While the PDF is helpful, we are not able to easily import it into our tool to create the symbol without extracting that info manually from the PDF. Is there an excel sheet version of this information?

Thank you for your help!

A. Kowalczyk

0 Kudos
Reply

1,198 Views
Hector_Villarruel
NXP TechSupport
NXP TechSupport

Hello @akowalczyk 

Hope this post finds you well,

Unfortunately we do not have available such excel file,

Nevertheless can provide the symbol file for the device,

Please note that in order to provide such a file it is necessary to create a technical support ticket and mention that the new case is related to this one.

You can create a new ticket using the technical support web located in the following link:

https://support.nxp.com/s/

Best Regards,

Hector Villarruel

 

0 Kudos
Reply

1,228 Views
Hector_Villarruel
NXP TechSupport
NXP TechSupport

Hello @akowalczyk 

Hope this post finds you well, 

The pinout list of the T1042 is located on pages 10-44 of QorIQ T1042, T1022 Data Sheet, Rev. 2, 06/2015.

Please find attached on this post the Data Sheet of the device.

BR,

Hector Villarruel Silvadoray 

0 Kudos
Reply