Hi NXP Team,
I have designed a custom board using T1042. I am using 2 PHYs with the ethernet interface. Currently, i am in testing phase of my board. How can i test whether the ethernet interface is working or not? Is there any protocol or software for this purpose? Any information regarding the query will be appreciated.
Use u-boot for data loading via TFTP. If there is no problem during data loading under u-boot, load Linux image (kernel, root file system and .dtb file).
There are a lot test programs under Linux. For example, see the following:
or
https://spindance.com/test-automation-embedded-part-1/
Look at also the following document:
Use this document as example for board testing.
Have a great day,
Pavel Chubakov
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------