T1042 eMMC usage in HS200 mode with 4-Bit configuration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

T1042 eMMC usage in HS200 mode with 4-Bit configuration

581 Views
ilhanbey
Contributor I

Dear Responsible,

In our new design we will use T1042. In this project we need to use eMMC with HS200 mode with 4-Bit configuration.

For this purpose after reading T1042 datasheet and Reference Manual; i have made search in NXP site and  i found AN4825.

But still not so clear to usage of "SDHC_CLK_SYNC_IN" and "SDHC_CLK_SYNC_OUT" signals. Especially in AN4825 @page 37 in Figure-13 SDHC_CLK_SYNC_IN signal is coming no where?

By the way could you pls also inform me about the real implementation of "SDHC_VS" signal? Do you have any reference design?

Thanks in advance.

Labels (1)
0 Kudos
1 Reply

497 Views
ufedor
NXP Employee
NXP Employee

I agree that the Figures 13 and 14 are ambiguous concerning the SDHC_CLK_SYNC_IN.
Please consider that Figure 12 showing correct loop of the SDHC_CLK_SYNC_OUT and SDHC_CLK_SYNC_IN.

0 Kudos