T1042 - compatible with DDR4 Component, MT40A1G16TD-062E-AUT:F?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

T1042 - compatible with DDR4 Component, MT40A1G16TD-062E-AUT:F?

跳至解决方案
811 次查看
trevorfox
Contributor III

Hi

I am designing a custom board using T1042 processor.

Would like to use high temp version of DDR4, specifically MT40A1G16TD-062E-AUT:F.

Can you verify if the DDR4 controller in the T series Qoriq PowerPC is compatible with this part?

 

0 项奖励
回复
1 解答
793 次查看
June_Lu
NXP TechSupport
NXP TechSupport

T1042 DDR controller is designed to support DDR4 SDRAMs that are compliant with JESD79-4 from September 2012. MT40A1G16TD-062E-AUT:F is supported. Refer to QorIQ T1040 Reference ManualTable 14-11. Supported SDRAM Device Configurations, DDR4

在原帖中查看解决方案

1 回复
794 次查看
June_Lu
NXP TechSupport
NXP TechSupport

T1042 DDR controller is designed to support DDR4 SDRAMs that are compliant with JESD79-4 from September 2012. MT40A1G16TD-062E-AUT:F is supported. Refer to QorIQ T1040 Reference ManualTable 14-11. Supported SDRAM Device Configurations, DDR4