Hi
I am designing a custom board using T1042 processor.
Would like to use high temp version of DDR4, specifically MT40A1G16TD-062E-AUT:F.
Can you verify if the DDR4 controller in the T series Qoriq PowerPC is compatible with this part?
解決済! 解決策の投稿を見る。
T1042 DDR controller is designed to support DDR4 SDRAMs that are compliant with JESD79-4 from September 2012. MT40A1G16TD-062E-AUT:F is supported. Refer to QorIQ T1040 Reference Manual, Table 14-11. Supported SDRAM Device Configurations, DDR4
T1042 DDR controller is designed to support DDR4 SDRAMs that are compliant with JESD79-4 from September 2012. MT40A1G16TD-062E-AUT:F is supported. Refer to QorIQ T1040 Reference Manual, Table 14-11. Supported SDRAM Device Configurations, DDR4