T1042 - compatible with DDR4 Component, MT40A1G16TD-062E-AUT:F?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

T1042 - compatible with DDR4 Component, MT40A1G16TD-062E-AUT:F?

Jump to solution
738 Views
trevorfox
Contributor III

Hi

I am designing a custom board using T1042 processor.

Would like to use high temp version of DDR4, specifically MT40A1G16TD-062E-AUT:F.

Can you verify if the DDR4 controller in the T series Qoriq PowerPC is compatible with this part?

 

0 Kudos
Reply
1 Solution
720 Views
June_Lu
NXP TechSupport
NXP TechSupport

T1042 DDR controller is designed to support DDR4 SDRAMs that are compliant with JESD79-4 from September 2012. MT40A1G16TD-062E-AUT:F is supported. Refer to QorIQ T1040 Reference ManualTable 14-11. Supported SDRAM Device Configurations, DDR4

View solution in original post

1 Reply
721 Views
June_Lu
NXP TechSupport
NXP TechSupport

T1042 DDR controller is designed to support DDR4 SDRAMs that are compliant with JESD79-4 from September 2012. MT40A1G16TD-062E-AUT:F is supported. Refer to QorIQ T1040 Reference ManualTable 14-11. Supported SDRAM Device Configurations, DDR4