I am planning to use T1042 QorIQ Processor for Control System applications.life of the part availability and the RTOS support.Whether Code warrior tool can be used for development without RTOS. Plese provide the Programming tool and the Debugging tool support for T1042 Processor.
please answer the end of life question. is it 5yrs, 10yrs, 15yrs, or more?
CodeWarrior for Power Architecture is a universal IDE which contains:
CodeWarrior® Development Suite for Networked Applications | NXP
Required hardware components are:
CodeWarrior TAP (CWH-CTP-BASE-HE):
https://www.nxp.com/design/software/development-software/codewarrior-development-tools/run-control-d...
CWTAP Probe Tip for PowerQUICC II/III, QorIQ MPUs (CWH-CTP-COP-YE):