Hi,
The "QorIQ T1040 Reference Manual, Rev. 0, 01/2015" shows SerDes lane assignment and multiplexing options in "Figure 31-1. Supported SerDes Options".
The SerDes mux configuration I am looking for is not listed.
For example, If I would need two PCIe x2, two sgmii and one SATA:
Would a SerDes mux configuration 0x41 be possible?
Or does Figure 31-1 show the only available ones?
Thanks,
lwn
Solved! Go to Solution.
Figure 31-1 shows the only available configurations. So other ones (like 0x41) are not allowed.
Regards,
Bulat
Hello lwn,
Any option not in the reference manual list of the Serdes protocol is not supported. Please choose one from the table.
You may leave some lanes not used.
Have a great day,
Lunmin
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Figure 31-1 shows the only available configurations. So other ones (like 0x41) are not allowed.
Regards,
Bulat