T1040d4 custom board without CPLD, JTAG programming issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

T1040d4 custom board without CPLD, JTAG programming issue

Jump to solution
1,408 Views
Wj_khi
Contributor II
Hi I have custom board designed using T1040d4 qoriq powerpc. My bareboard powerpc is currently power on using onboard power sequencing without using any CPLD. Right now i have no serial interface to monitor and debug it as both T1040 UART interfaced are attached with some other hardware over custom board. #Issue# when attached via CW usb tap its Jtag unable to program and flash bootloader via code warrior it shows " IR scan measure error" also "core not responding " in jtag log console.
0 Kudos
Reply
1 Solution
1 Reply