I am trying to boot T1040 from nand and use UBIFS. when booting from Nand, it boots well until the point of "mounting UBIFS". below is the error:
UBI: attaching mtd7 to ubi0
UBI error: validate_ec_hdr: bad VID header offset 512, expected 4096
UBI error: validate_ec_hdr: bad EC header
Erase counter header dump:
magic 0x55424923
version 1
ec 0
vid_hdr_offset 512
data_offset 1024
image_seq 2076921562
hdr_crc 0x951adef
erase counter header hexdump:
CPU: 2 PID: 1 Comm: swapper/0 Not tainted 3.12.19-rt30-QorIQ-SDK-V1.7+g6619b8b #6
Call Trace:
[c9081cd0] [c0006f50] show_stack+0x40/0x150 (unreliable)
[c9081d10] [c06e9a20] dump_stack+0x78/0xa0
[c9081d20] [c03a56ac] validate_ec_hdr+0xac/0x120
[c9081d30] [c03a6104] ubi_io_read_ec_hdr+0x184/0x240
[c9081d60] [c03aaf00] ubi_attach+0x180/0x14d0
[c9081de0] [c039fdf8] ubi_attach_mtd_dev+0x688/0xc80
[c9081e30] [c08e9348] ubi_init+0x274/0x30c
[c9081e80] [c00021a8] do_one_initcall+0x158/0x1b0
[c9081ef0] [c08cb8d0] kernel_init_freeable+0x134/0x1d0
[c9081f20] [c0002808] kernel_init+0x18/0x170
[c9081f40] [c000fe0c] ret_from_kernel_thread+0x5c/0x64
UBI error: ubi_io_read_ec_hdr: validation failed for PEB 0
UBI error: ubi_attach_mtd_dev: failed to attach mtd7, error -22
UBI error: ubi_init: cannot attach mtd7
UBIFS error (pid 1): ubifs_mount: cannot open "ubi0:rootfs", error -19
VFS: Cannot open root device "ubi0:rootfs" or unknown-block(0,0): error -19
Please append a correct "root=" boot option; here are the available partitions:
1f00 131072 mtdblock0 (driver?)
1f01 1536 mtdblock1 (driver?)
1f02 1024 mtdblock2 (driver?)
1f03 1024 mtdblock3 (driver?)
1f04 24576 mtdblock4 (driver?)
1f05 10240 mtdblock5 (driver?)
1f06 1024 mtdblock6 (driver?)
1f07 409600 mtdblock7 (driver?)
1f08 98304 mtdblock8 (driver?)
1f09 524288 mtdblock9 (driver?)
1f0a 65536 mtdblock10 (driver?)
Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(0,0)
CPU: 1 PID: 1 Comm: swapper/0 Not tainted 3.12.19-rt30-QorIQ-SDK-V1.7+g6619b8b #6
Call Trace:
[c9081dd0] [c0006f50] show_stack+0x40/0x150 (unreliable)
[c9081e10] [c06e9a20] dump_stack+0x78/0xa0
[c9081e20] [c06e7c9c] panic+0xd8/0x1fc
[c9081e70] [c08cbce4] mount_block_root+0x1b0/0x248
[c9081ed0] [c08cc064] prepare_namespace+0xa0/0x1d0
[c9081ef0] [c08cb958] kernel_init_freeable+0x1bc/0x1d0
[c9081f20] [c0002808] kernel_init+0x18/0x170
[c9081f40] [c000fe0c] ret_from_kernel_thread+0x5c/0x64
Rebooting in 180 seconds..
what I did was:
1.build kernel to support support UBIFS
2. build uboot to support UBIFS
3. set boot cmd to :
bootcmd=setenv bootargs noinitrd ip=off mem=256M rootwait=1 rw ubi.mtd=7,4096 rootfstype=ubifs root=ubi0:rootfs console=$consoledev,$baudrate $othbootargs;nand read.e $loadaddr $kernel_addr $kernel_size;nand read.e $fdtaddr $fdt_addr $fdt_size;bootm $loadaddr - $fdtaddr
4. modify fsl-image-core.bb script
add image file type:
IMAGE_FSTYPES = "ubi"
build rootfs: I got 2 images:
fsl-image-core-t1040rdb-20150408204106.rootfs.ubi
fsl-image-core-t1040rdb-20150408204106.rootfs.ubifs
I update rootfs partition mtdblock7 with " fsl-image-core-t1040rdb-20150408204106.rootfs.ubifs"
Is the anything else need to set up to make it work?
Thanks
leo
解決済! 解決策の投稿を見る。
Hello Leo Tao,
Please refer to the following procedure and check whether you missed something.
1. Kernel configuration
Device Drivers --->
<*> Memory Technology Device (MTD) support --->
< > Parallel port support --->
<*> Enable UBI - Unsorted block images --->
<*> NAND Device Support --->
File systems --->
[*] Miscellaneous filesystems --->
[*] Network File Systems --->
<*> UBIFS file system support
2. Please check whether ubi filesystem has been formatted and deployed correctly.
Format the mtd balock to UBI
root@p1010rdb-pb:ram# ubiformat /dev/mtdXX --yes
Where "XX" is the MTD device num
E.g:
root@p1010rdb-pb:ram# ubiformat /dev/mtd7 --yes
ubiformat: mtd7 (nand), size 58720256 bytes (56.0 MiB), 112 eraseblocks of 524288 bytes (512.0 KiB), min. I/O size 4096 bytes
libscan: scanning eraseblock 111 -- 100 % complete
ubiformat: 110 eraseblocks are supposedly empty
ubiformat: 2 bad eraseblocks found, numbers: 74, 75
ubiformat: formatting eraseblock 111 -- 100 % complete
Flash the ubi image into mtd block:
root@p1010rdb-pb:ram# ubiformat /dev/mtdXX -f ./rootfs.ubi
Where "XX" is the MTD device num
E.g:
ubiformat: mtd7 (nand), size 58720256 bytes (56.0 MiB), 112 eraseblocks of 524288 bytes (512.0 KiB), min. I/O size 4096 bytes
libscan: scanning eraseblock 111 -- 100 % complete
ubiformat: 110 eraseblocks have valid erase counter, mean value is 0
ubiformat: 2 bad eraseblocks found, numbers: 74, 75
ubiformat: flashing eraseblock 22 -- 100 % complete
ubiformat: formatting eraseblock 111 -- 100 % complete
3. Please check whether the ubi partition can be attached successfully.
root@p1021rdb:~# ubiattach /dev/ubi_ctrl -m XX
Where "XX" is the MTD device num
E.g:
root@p1010rdb-pb:ram# ubiattach /dev/ubi_ctrl -m 7
UBI: attaching mtd7 to ubi0
UBI: scanning is finished
UBI: volume 0 ("p1010rdb-rootfs") re-sized from 21 to 28 LEBs
UBI: attached mtd7 (name "NAND Compressed RFS Image", size 56 MiB) to ubi0
UBI: PEB size: 524288 bytes (512 KiB), LEB size: 516096 bytes
UBI: min./max. I/O unit sizes: 4096/4096, sub-page size 4096
UBI: VID header offset: 4096 (aligned 4096), data offset: 8192
UBI: good PEBs: 110, bad PEBs: 2, corrupted PEBs: 0
UBI: user volume: 1, internal volumes: 1, max. volumes count: 128
UBI: max/mean erase counter: 1/1, WL threshold: 4096, image sequence number: 1063368973
UBI: available PEBs: 0, total reserved PEBs: 110, PEBs reserved for bad PEB handling: 78
UBI: background thread "ubi_bgt0d" started, PID 2504
Check the ubi partition:
root@p1010rdb-pb:ram# mount -t ubifs ubi0_0 /mnt
UBIFS: background thread "ubifs_bgt0_0" started, PID 2507
UBIFS: mounted UBI device 0, volume 0, name "p1010rdb-rootfs"
UBIFS: LEB size: 516096 bytes (504 KiB), min./max. I/O unit sizes: 4096 bytes/4096 bytes
UBIFS: FS size: 9289728 bytes (8 MiB, 18 LEBs), journal size 4644865 bytes (4 MiB, 8 LEBs)
UBIFS: reserved for root: 0 bytes (0 KiB)
UBIFS: media format: w4/r0 (latest is w4/r0), UUID 9709D18F-23C6-4A52-9BF1-03EAB33C0B87, small LPT model
root@p1010rdb-pb:ram# mount
...
ubi0_0 on /mnt type ubifs (rw,relatime)
bin boot dev etc home lib linuxrc media mnt proc run sbin sys tmp usr var
4. Please check ubi rootfs bootarts
=>setenv bootargs ubi.mtd=<MTD_num> root=ubi0_0 rw rootfstype=ubifs console=ttyS0,115200 init=/init
=>tftpboot $loadaddr uImage-ubi.bin
=>tftpboot $fdtaddr l <dtb_file>
=>bootm $loadaddr - $fdtaddr
Have a great day,
Yiping
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello Leo Tao,
Please refer to the following procedure and check whether you missed something.
1. Kernel configuration
Device Drivers --->
<*> Memory Technology Device (MTD) support --->
< > Parallel port support --->
<*> Enable UBI - Unsorted block images --->
<*> NAND Device Support --->
File systems --->
[*] Miscellaneous filesystems --->
[*] Network File Systems --->
<*> UBIFS file system support
2. Please check whether ubi filesystem has been formatted and deployed correctly.
Format the mtd balock to UBI
root@p1010rdb-pb:ram# ubiformat /dev/mtdXX --yes
Where "XX" is the MTD device num
E.g:
root@p1010rdb-pb:ram# ubiformat /dev/mtd7 --yes
ubiformat: mtd7 (nand), size 58720256 bytes (56.0 MiB), 112 eraseblocks of 524288 bytes (512.0 KiB), min. I/O size 4096 bytes
libscan: scanning eraseblock 111 -- 100 % complete
ubiformat: 110 eraseblocks are supposedly empty
ubiformat: 2 bad eraseblocks found, numbers: 74, 75
ubiformat: formatting eraseblock 111 -- 100 % complete
Flash the ubi image into mtd block:
root@p1010rdb-pb:ram# ubiformat /dev/mtdXX -f ./rootfs.ubi
Where "XX" is the MTD device num
E.g:
ubiformat: mtd7 (nand), size 58720256 bytes (56.0 MiB), 112 eraseblocks of 524288 bytes (512.0 KiB), min. I/O size 4096 bytes
libscan: scanning eraseblock 111 -- 100 % complete
ubiformat: 110 eraseblocks have valid erase counter, mean value is 0
ubiformat: 2 bad eraseblocks found, numbers: 74, 75
ubiformat: flashing eraseblock 22 -- 100 % complete
ubiformat: formatting eraseblock 111 -- 100 % complete
3. Please check whether the ubi partition can be attached successfully.
root@p1021rdb:~# ubiattach /dev/ubi_ctrl -m XX
Where "XX" is the MTD device num
E.g:
root@p1010rdb-pb:ram# ubiattach /dev/ubi_ctrl -m 7
UBI: attaching mtd7 to ubi0
UBI: scanning is finished
UBI: volume 0 ("p1010rdb-rootfs") re-sized from 21 to 28 LEBs
UBI: attached mtd7 (name "NAND Compressed RFS Image", size 56 MiB) to ubi0
UBI: PEB size: 524288 bytes (512 KiB), LEB size: 516096 bytes
UBI: min./max. I/O unit sizes: 4096/4096, sub-page size 4096
UBI: VID header offset: 4096 (aligned 4096), data offset: 8192
UBI: good PEBs: 110, bad PEBs: 2, corrupted PEBs: 0
UBI: user volume: 1, internal volumes: 1, max. volumes count: 128
UBI: max/mean erase counter: 1/1, WL threshold: 4096, image sequence number: 1063368973
UBI: available PEBs: 0, total reserved PEBs: 110, PEBs reserved for bad PEB handling: 78
UBI: background thread "ubi_bgt0d" started, PID 2504
Check the ubi partition:
root@p1010rdb-pb:ram# mount -t ubifs ubi0_0 /mnt
UBIFS: background thread "ubifs_bgt0_0" started, PID 2507
UBIFS: mounted UBI device 0, volume 0, name "p1010rdb-rootfs"
UBIFS: LEB size: 516096 bytes (504 KiB), min./max. I/O unit sizes: 4096 bytes/4096 bytes
UBIFS: FS size: 9289728 bytes (8 MiB, 18 LEBs), journal size 4644865 bytes (4 MiB, 8 LEBs)
UBIFS: reserved for root: 0 bytes (0 KiB)
UBIFS: media format: w4/r0 (latest is w4/r0), UUID 9709D18F-23C6-4A52-9BF1-03EAB33C0B87, small LPT model
root@p1010rdb-pb:ram# mount
...
ubi0_0 on /mnt type ubifs (rw,relatime)
bin boot dev etc home lib linuxrc media mnt proc run sbin sys tmp usr var
4. Please check ubi rootfs bootarts
=>setenv bootargs ubi.mtd=<MTD_num> root=ubi0_0 rw rootfstype=ubifs console=ttyS0,115200 init=/init
=>tftpboot $loadaddr uImage-ubi.bin
=>tftpboot $fdtaddr l <dtb_file>
=>bootm $loadaddr - $fdtaddr
Have a great day,
Yiping
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello YiPing,
Thank you very much for your detailed information.
I understand you try to burn rootfs.ubi to Flash properly by using “ubiformat” from Liunx shell instead of using u-boot command “nand write”.
But I am not able to run the instruction below:
root@p1010rdb-pb:ram# ubiformat /dev/mtdXX -f ./rootfs.ubi
The problem is when I transfer rootfs.ubi from my host machine to target board T1040RDB, the rootfs image can’t be transferred completely.
Maximum size of file can be copied to Linux directory is about 23MB while the size of rootfs.ubi is about 50MB.
Is there anyway to enlarge linux directory size limit in bitbake?
Below is the error, after copy 23MB file to Linux, you don’t even have any room to create a mount point.
Thanks
Leo
root@t1040rdb:~# tftp 192.168.0.1
tftp> get /tftpboot/root.ubifs /home/root.ubifs
root@t1040rdb:~# ls -al /home
total 23924
drwxr-sr-x 3 root root 1024 Mar 27 19:22 .
drwxr-xr-x 18 root root 1024 Jan 1 1970 ..
drwxr-xr-x 2 root root 1024 Mar 25 22:55 root
-rw-rr 1 root root 24397824 Mar 27 19:25 root.ubifs
root@t1040rdb:~# mkdir /var/nfs
mkdir: cannot create directory '/var/nfs': No space left on device
Hello leo tao,
When ramdisk rootfs is generated, there is no much spare space allocated for /dev/root, you could copy a larger file into “/tmp” folder.
In addition, there is a limitation with tftp command, it cannot download a file over 32M, please try to use the following command instead.
busybox tftp -g -r /tftpboot/root.ubi 192.168.2.1
Have a great day,
Yiping
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------