T1040D4RDB fsl-image-full build fail

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

T1040D4RDB fsl-image-full build fail

1,616 次查看
wenjunzhu
Contributor I

Hi!

I an using SDK 2.0 and SDK 2.0-1703 updates to build packages for T1040D4RDB-64b. However, the process failed because 'gnulib' did not match any files known to git. I check on other boards forum and one of the forum says you try to find the .gitModules files and modify the URL, but I cannot exactly find that specific file or modules. Is there any solution to this problem?

Thank you!

Here is the log message:

WARNING: Host distribution "Ubuntu-16.04" has not been validated with this version of the build system; you may possibly experience unexpected failures. It is recommended that you use a tested distribution.
Loading cache: 100% |###########################################| ETA:  00:00:00
Loaded 6083 entries from dependency cache.
NOTE: Resolving any missing task queue dependencies

Build Configuration:
BB_VERSION        = "1.28.0"
BUILD_SYS         = "x86_64-linux"
NATIVELSBSTRING   = "Ubuntu-16.04"
TARGET_SYS        = "powerpc64-fsl-linux"
MACHINE           = "t1040d4rdb-64b"
DISTRO            = "fsl-qoriq"
DISTRO_VERSION    = "2.0"
TUNE_FEATURES     = "m64 fpu-hard e5500"
TARGET_FPU        = "hard"
meta             
meta-yocto       
meta-yocto-bsp    = "HEAD:9a211a4a2c1bfcb292dc97d8dcac149bca9e3f1b"
meta-oe          
meta-multimedia  
meta-gnome       
meta-networking  
meta-perl        
meta-python      
meta-ruby        
meta-filesystems 
meta-webserver   
meta-xfce         = "HEAD:dc5634968b270dde250690609f0015f881db81f2"
meta-freescale    = "HEAD:7facbdb726e2dda0515e084c2066a4b8dd99c6d2"
meta-freescale-internal = "HEAD:4829293f807e35a1111e79763294fc8b98b97810"
meta-freescale-extra = "HEAD:bee911b027e0480b034674d0ddee3fcb06d2e985"
meta-virtualization = "HEAD:042425c1d98bdd7e44a62789bd03b375045266f5"
meta-java         = "HEAD:8b776ac68f9af4596be3824152bcf0bc6b67fa1d"
meta-openstack   
meta-openstack-aio-deploy
meta-openstack-compute-deploy
meta-openstack-compute-test-config
meta-openstack-controller-deploy
meta-openstack-controller-test-config
meta-openstack-qemu
meta-openstack-swift-deploy
meta-cloud-services = "HEAD:d8bc0d92d0f741e2ea1e6d3d9bc6b7a091d03cfb"
meta-security     = "HEAD:f9367e71f923fc7d2fb600208e2b97535ea41777"
meta-nxp-npi-1703 = "jethro-sdk-v2.0-ga-17.03:d8f8d3a5d3ee18f881466938b847cef9b08c4a35"

NOTE: Preparing RunQueue
WARNING: /home/jeremy/QorIQ-SDK-V2.0-20160527-yocto/sources/meta-openembedded/meta-networking/recipes-support/netcf/netcf_git.bb.do_configure is tainted from a forced run
NOTE: Checking sstate mirror object availability (for 1974 objects)
NOTE: Executing SetScene Tasks
NOTE: Executing RunQueue Tasks
ERROR: Function failed: do_configure (log file is located at /home/jeremy/QorIQ-SDK-V2.0-20160527-yocto/build_t1040d4rdb-64b/tmp/work/ppc64e5500-fsl-linux/netcf/0.2.8+gitAUTOINC+9158278ad3-r0/temp/log.do_configure.2247)
ERROR: Logfile of failure stored in: /home/jeremy/QorIQ-SDK-V2.0-20160527-yocto/build_t1040d4rdb-64b/tmp/work/ppc64e5500-fsl-linux/netcf/0.2.8+gitAUTOINC+9158278ad3-r0/temp/log.do_configure.2247
Log data follows:
| DEBUG: Executing python function sysroot_cleansstate
| DEBUG: Python function sysroot_cleansstate finished
| DEBUG: SITE files ['endian-big', 'bit-64', 'powerpc-common', 'common-linux', 'common-glibc', 'powerpc-linux', 'powerpc64-linux', 'common']
| DEBUG: Executing shell function autotools_preconfigure
| DEBUG: Shell function autotools_preconfigure finished
| DEBUG: Executing python function autotools_copy_aclocals
| DEBUG: SITE files ['endian-big', 'bit-64', 'powerpc-common', 'common-linux', 'common-glibc', 'powerpc-linux', 'powerpc64-linux', 'common']
| DEBUG: Python function autotools_copy_aclocals finished
| DEBUG: Executing shell function do_configure
| ./bootstrap: Bootstrapping from checked-out netcf sources...
| ./bootstrap: consider installing git-merge-changelog from gnulib
| ./bootstrap: getting gnulib files...
| error: pathspec 'gnulib' did not match any file(s) known to git.
| WARNING: exit code 1 from a shell command.
| ERROR: Function failed: do_configure (log file is located at /home/jeremy/QorIQ-SDK-V2.0-20160527-yocto/build_t1040d4rdb-64b/tmp/work/ppc64e5500-fsl-linux/netcf/0.2.8+gitAUTOINC+9158278ad3-r0/temp/log.do_configure.2247)
ERROR: Task 4442 (/home/jeremy/QorIQ-SDK-V2.0-20160527-yocto/sources/meta-openembedded/meta-networking/recipes-support/netcf/netcf_git.bb, do_configure) failed with exit code '1'
NOTE: Tasks Summary: Attempted 2358 tasks of which 2348 didn't need to be rerun and 1 failed.
Waiting for 0 running tasks to finish:

Summary: 1 task failed:
  /home/jeremy/QorIQ-SDK-V2.0-20160527-yocto/sources/meta-openembedded/meta-networking/recipes-support/netcf/netcf_git.bb, do_configure
Summary: There were 2 WARNING messages shown.
Summary: There was 1 ERROR message shown, returning a non-zero exit code.

标签 (1)
标记 (1)
0 项奖励
回复
2 回复数

1,247 次查看
Pavel
NXP Employee
NXP Employee

Use Ubuntu 14. Do not use Ubuntu 16.

Usually the following command sequence is used for SDK installing under Ubuntu 14.04 64-bit:

  1. sudo apt-get install ubuntu-minimal ubuntu-standard patch vim-common sed wget subversion git-core coreutils libbonobo2-common unzip texi2html texinfo libsdl1.2-dev docbook-utils gawk python-pysqlite2 diffstat make gcc build-essential xz-utils g++ desktop-file-utils chrpath libgl1-mesa-dev libglu1-mesa-dev autoconf automake groff libtool xterm libncurses5-dev cvs tofrodos

 

  1. a) command: ls -l /bin/sh

                Message:  /bin/sh -> dash

  1. b) command: sudo dpkg-reconfigure dash

                Answer after password – No

                Message:

                Removing 'diversion of /bin/sh to /bin/sh.distrib by dash'

                Adding 'diversion of /bin/sh to /bin/sh.distrib by bash'

                Removing 'diversion of /usr/share/man/man1/sh.1.gz to /usr/share/man/man1/sh.distrib.1.gz by dash'

                Adding 'diversion of /usr/share/man/man1/sh.1.gz to /usr/share/man/man1/sh.distrib.1.gz by bash'

  1. c) command for checking: ls -l /bin/sh

                Message: /bin/sh -> bash

 

  1. mount SDK 2.0 .iso file
  2. cd <sdk-install-dir>.
  3. ./sources/meta-freescale/scripts/host-prepare.sh

Usually Linux recommends also run the following command: sudo usr/sbin/visudo

  1. bitbake fsl-image-minimal
  2. bitbake fsl-image-full

 

SDK 2.0-1703 is not needed if the T1040 is used. This update is needed for LS processors.

 
Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,247 次查看
patrickb-iss
Contributor I

I also had this issue, but solved it by modifying the netcf recipe to not use the default automake bootstrap bitbake class and instead bootstrap without using git.

Here's a patch for sources/meta-openembedded with my changes:

diff --git a/meta-networking/recipes-support/netcf/netcf_git.bb b/meta-networking/recipes-support/netcf/netcf_git.bb
index 26c738b..1eb9341 100644
--- a/meta-networking/recipes-support/netcf/netcf_git.bb
+++ b/meta-networking/recipes-support/netcf/netcf_git.bb
@@ -16,13 +16,29 @@ DEPENDS += "augeas libnl libxslt libxml2 gnulib"
 
 S = "${WORKDIR}/git"
 
-inherit gettext autotools-bootstrap pkgconfig systemd
+# inherit gettext autotools-bootstrap pkgconfig systemd
+inherit gettext autotools pkgconfig systemd
 
 EXTRA_OECONF_append_class-target = " --with-driver=redhat"
 
 PACKAGECONFIG ??= "${@bb.utils.contains("DISTRO_FEATURES", "systemd", "systemd", "", d)}"
 PACKAGECONFIG[systemd] = "--with-sysinit=systemd,--with-sysinit=initscripts,"
 
+do_configure_prepend() {
+ currdir=`pwd`
+ cd ${S}
+
+ # avoid bootstrap cloning gnulib on every configure, hence "--no-git".
+ cp -rf ${STAGING_DATADIR}/gnulib ${S}
+
+ # --force to avoid errors on reconfigure e.g if recipes changed we depend on
+ # | bootstrap: running: libtoolize --quiet
+ # | libtoolize: error: 'libltdl/COPYING.LIB' exists: use '--force' to overwrite
+ # | ...
+ ./bootstrap --force --no-git --gnulib-srcdir=gnulib
+ cd $currdir
+}
+
 do_install_append() {
 if ${@base_contains('DISTRO_FEATURES', 'systemd', 'true', 'false', d)}; then
 install -d ${D}${systemd_unitdir}/system
0 项奖励
回复