Hi,
I want to enable some more chip selects from IFC controller. Tried to make changes in u-boot also, but its got hanged.
Here are the changes made by me,
1) T104xRDB.h
#define CONFIG_SYS_RAYCOM1_BASE 0xFF900000
#define CONFIG_SYS_RAYCOM1_BASE_PHYS (0xf00000000ull | CONFIG_SYS_RAYCOM1_BASE)
#define CONFIG_SYS_CSPR3_EXT (0xf)
#define CONFIG_SYS_CSPR3 (CSPR_PHYS_ADDR(CONFIG_SYS_RAYCOM1_BASE_PHYS) \
| CSPR_PORT_SIZE_8 \
| CSPR_MSEL_GPCM \
| CSPR_V)
#define CONFIG_SYS_AMASK3 IFC_AMASK(64*1024)
#define CONFIG_SYS_CSOR3 0x0
/* RAYCOM1 Timing parameters for IFC CS2 */
#define CONFIG_SYS_CS3_FTIM0 (FTIM0_GPCM_TACSE(0x0e) | \
FTIM0_GPCM_TEADC(0x0e) | \
FTIM0_GPCM_TEAHC(0x0e))
#define CONFIG_SYS_CS3_FTIM1 (FTIM1_GPCM_TACO(0x0e) | \
FTIM1_GPCM_TRAD(0x1f))
#define CONFIG_SYS_CS3_FTIM2 (FTIM2_GPCM_TCS(0x0e) | \
FTIM2_GPCM_TCH(0x0) | \
FTIM2_GPCM_TWP(0x1f))
#define CONFIG_SYS_CS3_FTIM3 0x0
2) tlb.c
#ifdef CONFIG_SYS_RAYCOM1_BASE
SET_TLB_ENTRY(1, CONFIG_SYS_RAYCOM1_BASE, CONFIG_SYS_RAYCOM1_BASE_PHYS,
MAS3_SW|MAS3_SR, MAS2_I|MAS2_G,
0, 14, BOOKE_PAGESZ_256K, 1),
#endif
3) law.c
#ifdef CONFIG_SYS_RAYCOM1_BASE_PHYS
SET_LAW(CONFIG_SYS_RAYCOM1_BASE_PHYS, LAW_SIZE_64K, LAW_TRGT_IF_IFC),
#endif
pls let me know where im doing wrong. Any more configuration is required???
--
Gourav
Hello Gourav Jain,
What kind of device is configured at IFC CS2? How do you decide IFC Timing parameters for this device?
Have a great day,
Yiping
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Yiping,
Issue got resolved. It was there because of IFC clock, which was higher than expected for end device.
thanks for you interest in my post..
--
Gourav