T1040 802.1x l2 switch port configuration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

T1040 802.1x l2 switch port configuration

748 Views
richard_bouck
Contributor I

I am trying to configure the l2 switch in a T1040D4RDB for 802.1x port authentication using the l2switch-cfg commands.

I have tried the "auth" command without success:

   l2switch-cfg set auth both port <port_no>

I don't see a way to configure the radius-server on the l2switch as recommended in the "T1040 L2Switch Software Support" document:T1040 L2Switch Software Support 

From section - 4.2 "802.1 X NetWork Access Server Configuration"

On the target board

(config)# radius-server key 111111

(config)# radius-server host 192.85.1.1

What l2switch-cfg commands should be used to configure 802.1x port authentication?  Or is there a better way to configure the l2 switch to support 802.1x port authentication.

0 Kudos
1 Reply

569 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Richard Bouck,

Port authentication is not supported by command l2switch-cfg in Freescale SDK.

Please refer to Fig.2 in T1040 L2Switch Software Support, the user could use SMBStax L2 Switch Stack to implement port authentication function, which is a binary package outside the Linux SDK.

Thanks,

Yiping

0 Kudos