T1024 and T4240 are foot print compatible or not

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

T1024 and T4240 are foot print compatible or not

462 Views
kamlendrachandr
Contributor I

T1024 and T4240 are foot print compatible or not

0 Kudos
Reply
1 Reply

377 Views
alexander_yakov
NXP Employee
NXP Employee

No, these devices are not pin compatible, they have different number of pins - 780 pins for T1024 and 1932 pins for T4240.


Have a great day,
Alexander

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply