Hi,
We have confirmed the problem is caused by the incorrect setting for RCW bits 321 (UC1_CTSB_CDB_SEL) bit 322 (UC3_CTSB_CDB_SEL). I have manually patched the data to set these bits to '1' (i.e. to disable the extra flow control pins), and updated the CRC_Check command. After the system boot, the UCC communication commenced as expected.
It appears the QCVS tool PBL function is ignoring the project settings for UC1_CTSB_CDB_SEL and UC3_CTSB_CDB_SEL.
The tool version used to created the PBL is:
CodeWarrior Development Studio for Power Architecture
Version: 10.5.2
Build: 160608
QorIQ Configuration and Validation Suite
Version 4.5.0
Build: 0001-20160210