T1024 IFC connection with MRAM(SRAM)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

T1024 IFC connection with MRAM(SRAM)

跳至解决方案
2,288 次查看
safeerkt
Contributor II

Hi ,

We are planning to use QorIQ T1024 processor in one of our design.We want to interface a MRAM(SRAM archit) to the processor through IFC.We have a 4MBit MRAM with 19 address line and 8 data bit.could you please help me with the address and data mapping from processor to the MRAM part? Which all address and DA lines should I use and how should i map it?

Many Thanks,

Safeer.

标签 (1)
1 解答
1,936 次查看
alexander_yakov
NXP Employee
NXP Employee

Please look T1024 Reference Manual, Figure 23-65 "IFC to 8-bit NOR device interface" for example SRAM-like device connection. Please note reversal mapping - AD[0:7] to D[7:0] and AD[0:15]+ADDR[16:31] to A[31:0].


Have a great day,
Alexander

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

4 回复数
1,936 次查看
safeerkt
Contributor II

Hi Alexander,

Thank you very much for your support.

Just one more clarification,

In our SRAM part we have 19 address lines.So can I follow the below address mapping?

 T1024 side                            SRAM side

-----------------                        ------------------

ADDR[16:31]                        A[15:0]

AD[12:15]                             A[19:16]

Could you please confirm this?

Many Thanks,

Safeer.

0 项奖励
回复
1,936 次查看
alexander_yakov
NXP Employee
NXP Employee

Yes, I do not see anything incorrect.

1,936 次查看
safeerkt
Contributor II

Thanks Mr.Alexander.

0 项奖励
回复
1,937 次查看
alexander_yakov
NXP Employee
NXP Employee

Please look T1024 Reference Manual, Figure 23-65 "IFC to 8-bit NOR device interface" for example SRAM-like device connection. Please note reversal mapping - AD[0:7] to D[7:0] and AD[0:15]+ADDR[16:31] to A[31:0].


Have a great day,
Alexander

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------