T1024 DDR

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

T1024 DDR

跳至解决方案
1,629 次查看
BharathiG
Contributor I

Hi,

 

During the DDR initialization software is setting D_INIT bit and after initialization is done software waits for this bit to be cleared. Hardware will clear this bit after the initialization is complete.  Clearing of D_INIT bit is consistent for all T1024 hardware’s or it will changing with variation of environmental factor (temperature or electromagnetic effect) or any other factors?

BharathiG_1-1660727558895.png

 

0 项奖励
回复
1 解答
1,595 次查看
yipingwang
NXP TechSupport
NXP TechSupport

The clearing of D_INIT bit is done 100% of time by HW if DDR initialization completes.

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,565 次查看
BharathiG
Contributor I

I accept what you said and we are seeing the clearing of D_INIT bit by hardware. Powerup to powerup will their be any variations (timing variations) in clearing this bit ? Will it be consistently clearing the bit?

0 项奖励
回复
1,544 次查看
yipingwang
NXP TechSupport
NXP TechSupport

For the same board type (same HW and SW/settings), the time it takes to clear the D_INIT would be constantly the same.

0 项奖励
回复
1,596 次查看
yipingwang
NXP TechSupport
NXP TechSupport

The clearing of D_INIT bit is done 100% of time by HW if DDR initialization completes.

0 项奖励
回复