T1022 SerDes Recommended Input Voltage

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

T1022 SerDes Recommended Input Voltage

Jump to solution
1,770 Views
jack_mcculloch
Contributor I

Hi,

We are looking to drive a SFP directly from a SerDes output on the T1022. But there is some confusion on what the recommended signals levels for this interface is.

The T1022 has a max VRX-DIFFp-p of 1.6V in 1000Base-KX mode (table 44) my understanding is that will equate to an allowable 0.8V single ended voltage swing on a SerDes input?

The SFP MSA states that a SFP can output a signal that is 2V differential (1v singled ended). This exceeds the max of the T1022, but note 1 on table 44 refers to table 3 for recommended operating conditions. Table 3 states SerDes inputs have a recommend range of GND to S1VDD this suggests that the SFP would be ok?

Would this also apply when operating in SGMII mode (table 39)?

Thanks,

Bob

Labels (1)
Tags (2)
0 Kudos
Reply
1 Solution
1,703 Views
Bulat
NXP Employee
NXP Employee

Table 3 states that Serdes inputs are tolerant to GND to S1VDD signals level, so 1V is ok.
Table 44 directly states/repeats IEEE 802.3 specifications for 1000Base-KX receiver (clause 70.7.2).
Table 43 provides IEEE 802.3 specifications for 1000Base-KX transmitter (clause 70.7.1), here you can also see 1600mV maximum. If a SFP outputs VTX-DIFFp-p 2V (2000mV instead of 1600mV), it does not comply with the standard. However there is no electrical problem from the T1022 side due to table 3 specs.
Same applies to SGMII mode.

Regards,

Bulat

View solution in original post

1 Reply
1,704 Views
Bulat
NXP Employee
NXP Employee

Table 3 states that Serdes inputs are tolerant to GND to S1VDD signals level, so 1V is ok.
Table 44 directly states/repeats IEEE 802.3 specifications for 1000Base-KX receiver (clause 70.7.2).
Table 43 provides IEEE 802.3 specifications for 1000Base-KX transmitter (clause 70.7.1), here you can also see 1600mV maximum. If a SFP outputs VTX-DIFFp-p 2V (2000mV instead of 1600mV), it does not comply with the standard. However there is no electrical problem from the T1022 side due to table 3 specs.
Same applies to SGMII mode.

Regards,

Bulat