SerDes i/o voltage compatibility

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SerDes i/o voltage compatibility

641 Views
faizmajeed
Contributor III

Hi!

I am using T1042 and using 1st four Lanes of SerDes as PCIe. These PCIe Lanes are connected to PCIe switch which communicate with i/o volatge of 3.3V. I am confused with voltage compatibility.

can i connect this PCIe switch directly to SerDes pins or i need any voltage converter?

Thank You

Labels (1)
2 Replies

503 Views
ufedor
NXP Employee
NXP Employee

The T1042 must be connected so that its Data Sheet requirements and specifications were met.

For the SerDes PCIe inputs characteristics please refer to the section "3.22.4.3 PCI Express DC physical layer receiver specifications".

503 Views
faizmajeed
Contributor III

Thanx Ufedor

0 Kudos