SerDes PEXx Protocol Control Register 7 Reset Value

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SerDes PEXx Protocol Control Register 7 Reset Value

872 次查看
brianross
Contributor I

It appears in the QorIQ T2080 Reference Manual, Rev. 3, 11/2016 that the SerDesx_PEXnCR7[EQ_EN] reset value is 0, but when I check with an emulator it looks to be set.  Is the reset value listed in the reference manual incorrect for this register?  The full read yielded 0x90C0_0003 for SerDes1_PEX[0:3].

0 项奖励
回复
2 回复数

785 次查看
brianross
Contributor I

I double-checked and made sure I performed a read returning big-endian format and I still get 0x90C00003 so it appears like SerDesx_PEXnCR7[EQ_EN] should be 1 by default.  I'm having trouble with PCIe Gen3 and want to make sure the autonomous equalization is enabled.

0 项奖励
回复

785 次查看
ufedor
NXP Employee
NXP Employee

Please note that the register is big-endian, so the value is 0x300C090 - i.e. EQ_EN is 0.

0 项奖励
回复