SGMII to SGMII connection in T1022

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SGMII to SGMII connection in T1022

Jump to solution
841 Views
roya_azimi93
Contributor II

Hi,

in my custom design, I have two T1022 and I want to have SGMII  to SGMII communication between them. 

Is SGMII-SGMII allowable connection in T1022 by crossing RX/TX signals?

Regards,

Roya.

 

 

 

0 Kudos
1 Solution
825 Views
r8070z
NXP Employee
NXP Employee

Yes SGMII-SGMII connection is possible. Using 1000Base-KX is recommended. 1000Base-KX is supported on all SGMII lanes of the T1022.

View solution in original post

0 Kudos
1 Reply
826 Views
r8070z
NXP Employee
NXP Employee

Yes SGMII-SGMII connection is possible. Using 1000Base-KX is recommended. 1000Base-KX is supported on all SGMII lanes of the T1022.

0 Kudos