Rgmii to Rdmii connection in T1023

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Rgmii to Rdmii connection in T1023

697件の閲覧回数
gauravverma
Contributor II

Can we make communication between two T1023 processor using direct  Rgmii interface?

Is this configuration is supported by software as well ?

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 返信

579件の閲覧回数
r8070z
NXP Employee
NXP Employee


Have a great day,

Yes, it is pssoble to connect two T1023 processors via RGMII directly (MAC-to-MAC connection). Software should be configured for fixed link when auto negation is disabled.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信