Can we make communication between two T1023 processor using direct Rgmii interface?
Is this configuration is supported by software as well ?
Have a great day,
Yes, it is pssoble to connect two T1023 processors via RGMII directly (MAC-to-MAC connection). Software should be configured for fixed link when auto negation is disabled.
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------