RCW Problem with T1024 new design

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RCW Problem with T1024 new design

516 Views
josephvogl
Contributor I

We have a new design using a T1024 and are stuck.    

The processor is connected to an FPGA on the IFC bus.

We setup the RCW source to be 0_0010 0101, which should tell it to get the RCW from the IFC bus.

Using an emulator we verified that the POR Status Register 1 showed that value, so we know we have that right.

What address  will the processor go to for the RCW words over the IFC bus after it gets the RCW source?   We see address 0000 on AD[0..15] and A[16..31] = 000E.  The very next address is 4E on A[16..31].  

Can you please explain what we are seeing here?  We expected to see accesses to 00000000 for the RCW words which is where we put the data.   

Regards,


Joe Vogl

Labels (1)
0 Kudos
1 Reply

416 Views
ufedor
NXP Employee
NXP Employee

Is IFC_A31 connected to the A0 of the FPGA?

Is the FPGA data bus 16-bit-wide?

If both "yes" - then RCW source has to be 0_0010 0111.

0 Kudos