Question about T2080 Clock Speeds

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Question about T2080 Clock Speeds

984 Views
louis_lo
Contributor I

As advertised on the T2080RDB brochure, it can run from 1200MHz up to 1800 MHz. 

Out of the box the T2080RDB is running at around 1800MHz, as displayed through the generic uboot when connected via UART.

Is there any way to tweak this such that the clock speed can be lowered, say to 1200MHz?

I heard from a colleague that there needs to be an RCW tweak. I'm not sure what that is as I'm fairly new to all this.

Please advise.

Thanks!

Labels (1)
0 Kudos
Reply
1 Reply

943 Views
ufedor
NXP Employee
NXP Employee

The issue is already investigated as Technical Case #00286662

0 Kudos
Reply