Qoriq t1024 bareboard programming guide

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Qoriq t1024 bareboard programming guide

2,893 Views
leventkarakaya
Contributor I

Hello

Is there any programming guide, manual, or tutorial for programming bareboard applications on Qoriq t1024 processor?

Best regards

Labels (1)
0 Kudos
Reply
7 Replies

2,613 Views
ufedor
NXP Employee
NXP Employee

Do you mean application development or on-board flash programming?

0 Kudos
Reply

2,613 Views
slimSHA
Contributor III

can u please tell how to do onboard flashing

0 Kudos
Reply

2,613 Views
leventkarakaya
Contributor I

I mean bareboard application development. I dont want to use Linux. Instead, I will program the flash. It was named as Bareboard application in CodeWarrior. But, I could not find any programming guide or tutorial on how to program bareboard application. Where can I find such materials?

Regards

0 Kudos
Reply

2,613 Views
ufedor
NXP Employee
NXP Employee

Information about bareboard applications is provided in the CodeWarrior Development Studio for Power Architecture Processors Targeting Manual (\CW_PA_v10.5.1\PA\Help\PDF\Targeting_PA_Processors.pdf) and, also, CodeWarrior installation contains Bareboard Example project.

0 Kudos
Reply

2,613 Views
leventkarakaya
Contributor I

Hi

Thank you for information.

Document contains information on debugging, and creating projects in CWPA. But I am looking for a programming guide for bareboard applications. For example, how can I create an ethernet TCP socket?, how can I communicate with CPLD?, etc.

Do you know such a document?

Best regards

0 Kudos
Reply

2,613 Views
ufedor
NXP Employee
NXP Employee

> how can I create an ethernet TCP socket?, how can I communicate with CPLD?

There is no such guide.

Possible reference could be U-Boot source code.

0 Kudos
Reply

2,613 Views
leventkarakaya
Contributor I

Thank you for your help.

Best regards

0 Kudos
Reply