QorIQ T1040 Hardcoded RCW usage in "Single Oscillator Source" Reference Clock mode

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

QorIQ T1040 Hardcoded RCW usage in "Single Oscillator Source" Reference Clock mode

跳至解决方案
2,045 次查看
fdm
Contributor IV

Hi,

I'm planning to use the "Single Oscillator Source" Reference Clock mode in the T1040 based custom board currently in development.

Is it possible to use a "Hardcoded RCW" option in order to program the NOR and/or NAND flash with CW TAP during board bring-up if only DIFF_SYSCLK=100MHz is supplied and the DDRCLK dedicated pin is not connected at all?

BR,

   Denis

标签 (1)
0 项奖励
回复
1 解答
1,742 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Hello Denis Finogeev,

In CodeWarrior project you could select SRAM initialization file to initialize the target and download flash algorithm in SRAM to program NOR/NAND Flash.

When you create a bareboard CodeWarrior project, please select "Download SRAM" or "Connect SRAM" Launch configuration in the panel "Debug Target Settings".


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,743 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Hello Denis Finogeev,

In CodeWarrior project you could select SRAM initialization file to initialize the target and download flash algorithm in SRAM to program NOR/NAND Flash.

When you create a bareboard CodeWarrior project, please select "Download SRAM" or "Connect SRAM" Launch configuration in the panel "Debug Target Settings".


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复