QorIQ T1040 Hardcoded RCW usage in "Single Oscillator Source" Reference Clock mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

QorIQ T1040 Hardcoded RCW usage in "Single Oscillator Source" Reference Clock mode

ソリューションへジャンプ
2,132件の閲覧回数
fdm
Contributor IV

Hi,

I'm planning to use the "Single Oscillator Source" Reference Clock mode in the T1040 based custom board currently in development.

Is it possible to use a "Hardcoded RCW" option in order to program the NOR and/or NAND flash with CW TAP during board bring-up if only DIFF_SYSCLK=100MHz is supplied and the DDRCLK dedicated pin is not connected at all?

BR,

   Denis

ラベル(1)
0 件の賞賛
返信
1 解決策
1,829件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello Denis Finogeev,

In CodeWarrior project you could select SRAM initialization file to initialize the target and download flash algorithm in SRAM to program NOR/NAND Flash.

When you create a bareboard CodeWarrior project, please select "Download SRAM" or "Connect SRAM" Launch configuration in the panel "Debug Target Settings".


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,830件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello Denis Finogeev,

In CodeWarrior project you could select SRAM initialization file to initialize the target and download flash algorithm in SRAM to program NOR/NAND Flash.

When you create a bareboard CodeWarrior project, please select "Download SRAM" or "Connect SRAM" Launch configuration in the panel "Debug Target Settings".


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信