QorIQ T1040 Hardcoded RCW usage in "Single Oscillator Source" Reference Clock mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

QorIQ T1040 Hardcoded RCW usage in "Single Oscillator Source" Reference Clock mode

Jump to solution
2,084 Views
fdm
Contributor IV

Hi,

I'm planning to use the "Single Oscillator Source" Reference Clock mode in the T1040 based custom board currently in development.

Is it possible to use a "Hardcoded RCW" option in order to program the NOR and/or NAND flash with CW TAP during board bring-up if only DIFF_SYSCLK=100MHz is supplied and the DDRCLK dedicated pin is not connected at all?

BR,

   Denis

Labels (1)
0 Kudos
Reply
1 Solution
1,781 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Denis Finogeev,

In CodeWarrior project you could select SRAM initialization file to initialize the target and download flash algorithm in SRAM to program NOR/NAND Flash.

When you create a bareboard CodeWarrior project, please select "Download SRAM" or "Connect SRAM" Launch configuration in the panel "Debug Target Settings".


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,782 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Denis Finogeev,

In CodeWarrior project you could select SRAM initialization file to initialize the target and download flash algorithm in SRAM to program NOR/NAND Flash.

When you create a bareboard CodeWarrior project, please select "Download SRAM" or "Connect SRAM" Launch configuration in the panel "Debug Target Settings".


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply