I'm generatin a new RCW with QCVS 4.5 for a T2080 board.
When I try to configure RCW_SRC, PBI_SRC and BOOT_LOC to NOR Flash, QCVS shows an error, why?
When I change PBI_SRC or BOOT_LOC to another interface there is no error.
If I try the same configuration with previous versions of QVCS (4.2.1) there is no error for this configuration.
Ok, after update no error is show.
Thank you.
De: addiyi
Enviado el: lunes, 30 de mayo de 2016 13:23
Para: Hernández Sánchez, Sergio
Asunto: Re: - QCVS error configuring NOR FLASH
NXP Community <https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>
QCVS error configuring NOR FLASH
reply from Adrian-Mihai Stoica<https://community.nxp.com/people/addiyi?et=watches.email.thread> in QorIQ Processing Platforms - View the full discussion<https://community.nxp.com/message/655533?et=watches.email.thread#comment-655533>
Ok, but why it is considered an ERROR, I think it is a valid configuration.
De: addiyi
Enviado el: lunes, 30 de mayo de 2016 9:38
Para: Hernández Sánchez, Sergio
Asunto: Re: - QCVS error configuring NOR FLASH
NXP Community <https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>
QCVS error configuring NOR FLASH
reply from Adrian-Mihai Stoica<https://community.nxp.com/people/addiyi?et=watches.email.thread> in QorIQ Processing Platforms - View the full discussion<https://community.nxp.com/message/655446?et=watches.email.thread#comment-655446>
I’ve selected V1.1
PBL generated is attached to this email.
De: addiyi
Enviado el: lunes, 30 de mayo de 2016 10:15
Para: Hernández Sánchez, Sergio
Asunto: Re: - QCVS error configuring NOR FLASH
NXP Community <https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>
QCVS error configuring NOR FLASH
reply from Adrian-Mihai Stoica<https://community.nxp.com/people/addiyi?et=watches.email.thread> in QorIQ Processing Platforms - View the full discussion<https://community.nxp.com/message/655496?et=watches.email.thread#comment-655496>
I’m using eclipse version installed in VirtualBox provided by NXP witk SDK 1.9
De: addiyi
Enviado el: lunes, 30 de mayo de 2016 12:56
Para: Hernández Sánchez, Sergio
Asunto: Re: - QCVS error configuring NOR FLASH
NXP Community <https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>
QCVS error configuring NOR FLASH
reply from Adrian-Mihai Stoica<https://community.nxp.com/people/addiyi?et=watches.email.thread> in QorIQ Processing Platforms - View the full discussion<https://community.nxp.com/message/655531?et=watches.email.thread#comment-655531>