Hi,
I want the specific instruction to access uart transmitter to print char in console in u-boot. I don't to know what specific command want to use for this.
steps,
1. Load register to UART transmit address
2. Store the char in the register
3. Print the char when uboot-debugging
Regards, VinothS
解決済! 解決策の投稿を見る。
Look at the Section 3.4.3.2 of the e6500 Core Reference Manual:
https://www.nxp.com/docs/en/reference-manual/E6500RM.pdf
See also the Chapter 5.6.1.2.1 of the EREF:
https://www.nxp.com/webapp/Download?colCode=EREF_RM&location=null
See also u-boot readme file:
https://git.denx.de/?p=u-boot.git;a=blob_plain;f=README;hb=HEAD
Find the " "Hello World" Demo:" in this file. This example contains printing from u-boot.
Have a great day,
Pavel Chubakov
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Look at the Section 3.4.3.2 of the e6500 Core Reference Manual:
https://www.nxp.com/docs/en/reference-manual/E6500RM.pdf
See also the Chapter 5.6.1.2.1 of the EREF:
https://www.nxp.com/webapp/Download?colCode=EREF_RM&location=null
See also u-boot readme file:
https://git.denx.de/?p=u-boot.git;a=blob_plain;f=README;hb=HEAD
Find the " "Hello World" Demo:" in this file. This example contains printing from u-boot.
Have a great day,
Pavel Chubakov
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Pavel,
Thank you for your reply.
But, I am working on the fresh board. We flashed u-boot alone with hard-coded RCW and we start u-boot debugging.
Please checkout this thread,
Lauterbach Trace32 Debugger with T4160RDB-64b
Thanks & Regards,
VinothS