Plan 9 resource sharing on T1040

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Plan 9 resource sharing on T1040

1,053件の閲覧回数
piddy
Contributor II

Hello everybody,

i am back once again with a question :smileywink:

I work on virtualization on a T1040RDB PPC platform, using KVM/QEMU.

Almost everything works now, but i ran into this. I want to try and pass on a shared folder from host to guest using.

I followed this:

Documentation/9psetup - QEMU

But i keep on getting the error

"Parameter driver expects device type"

Did i miss some kernel configs? Is this a bug?

If anyone can help, it would be amazing.

thanks already, and also thanks for the help before.

ラベル(1)
タグ(4)
0 件の賞賛
返信
1 返信

876件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello Piddy,

Please try to build qemu with "virtfs" enabled.


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信