Plan 9 resource sharing on T1040

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Plan 9 resource sharing on T1040

1,055 Views
piddy
Contributor II

Hello everybody,

i am back once again with a question :smileywink:

I work on virtualization on a T1040RDB PPC platform, using KVM/QEMU.

Almost everything works now, but i ran into this. I want to try and pass on a shared folder from host to guest using.

I followed this:

Documentation/9psetup - QEMU

But i keep on getting the error

"Parameter driver expects device type"

Did i miss some kernel configs? Is this a bug?

If anyone can help, it would be amazing.

thanks already, and also thanks for the help before.

Labels (1)
Tags (4)
0 Kudos
Reply
1 Reply

878 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Piddy,

Please try to build qemu with "virtfs" enabled.


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply