I am working with the SerDes module of the T1042 processor and would like to perform both internal and external loopback tests to validate its functionality. Could you provide guidance on the following:
Internal Loopback:
- What are the steps to configure and execute an internal loopback test on the SerDes module of the T1042 processor?
- Which specific SerDes registers or settings need to be adjusted for this test?
- How can I verify the test results to confirm the SerDes is operating correctly in internal loopback mode?
External Loopback:
- How can I set up an external loopback test for the SerDes module?
- What external connections or configurations are required for this test?
- Are there specific diagnostics or tools recommended to verify data integrity during the external loopback test?
Any detailed steps, register settings, or troubleshooting tips for performing these loopback tests would be greatly appreciated.
Thank you!