I am using a 64 bit memory FPGA connected by PCI in my T2080rdb. I am using the next function in a device driver
0002:01:00.0 Memory controller: Xilinx Corporation Device 7022 Subsystem: Xilinx Corporation Device
0007 Flags: bus master, fast devsel, latency 0
Memory at <ignored> (64-bit, prefetchable)
Memory at c40000000 (64-bit, prefetchable) [size=64K]
Capabilities: [40] Power Management version 3
Capabilities: [48] MSI: Enable- Count=1/8 Maskable- 64bit+
Capabilities: [60] Express Endpoint, MSI 00
Capabilities: [100] Device Serial Number 00-00-00-00-00-00-00-00 however, when I use the next functions in my device driver:
unsigned long pci_resource_[start|len|end|flags](struct pci_dev *pdev, int bar);
I have got the next result:
______BAR0______
The value of pci_resource_start is: 0x0
The value of pci_resource_len is: 0x0
However, when I use the same device driver in a PCI device driver that use 32 bit memory, I have got:
______BAR0______
The value of pci_resource_start is: 0xc20000000
The value of pci_resource_len is: 0x100000
any idea why is it happening this?
BR.
thank very much for your answer. That is true, however it must be a problem when a PCI device has a 64 bit memory.
Using the next function:
unsigned long pci_resource_[start|len|end|flags](struct pci_dev *pdev, int bar);
I have got the next result:
______BAR0______
The value of pci_resource_start is: 0x0
The value of pci_resource_len is: 0x0
However, when I use the same device driver in a PCI device driver that use 32 bit memory, I have got:
______BAR0______
The value of pci_resource_start is: 0xc20000000
The value of pci_resource_len is: 0x100000
I change dbt in other to say to the kernel that it is a 64 bit memory. But does not work. You can see:
PCI addresses are 64 bits wide, and are encoded into phys.mid and phys.low. However, the really interesting things are in phys.high which is a bit field:
Any idea?
U-Boot 2015.01+SDKv1.9+geb3d4fc (Apr 28 2016 - 09:54:26)
CPU0: T2080E, Version: 1.1, (0x85380011)
Core: e6500, Version: 2.0, (0x80400120)
Clock Configuration:
CPU0:1799.820 MHz, CPU1:1799.820 MHz, CPU2:1799.820 MHz, CPU3:1799.820 MHz,
CCB:599.940 MHz,
DDR:933.310 MHz (1866.620 MT/s data rate) (Asynchronous), IFC:149.985 MHz
FMAN1: 699.930 MHz
QMAN: 299.970 MHz
PME: 599.940 MHz
L1: D-cache 32 KiB enabled
I-cache 32 KiB enabled
Reset Configuration Word (RCW):
00000000: 1207001b 15000000 00000000 00000000
00000010: 66150002 00000000 e8104000 c1000000
00000020: 00800000 00000000 00000000 000307fc
00000030: 00000000 00000000 00000000 00000004
Board: T2080RDB, Board rev: 0x01 CPLD ver: 0x03, boot from SD/MMC
SERDES Reference Clocks:
SD1_CLK1=156.25MHZ, SD1_CLK2=100.00MHZ
SD2_CLK1=100.00MHZ, SD2_CLK2=100.00MHZ
I2C: ready
SPI: ready
DRAM: Detected UDIMM D3XP56082XL10AA
4 GiB (DDR3, 64-bit, CL=13, ECC on)
Flash: 128 MiB
L2: 2 MiB enabled
Corenet Platform Cache: 512 KiB enabled
Using SERDES1 Protocol: 102 (0x66)
Using SERDES2 Protocol: 21 (0x15)
SEC0: RNG instantiated
NAND: 512 MiB
MMC: FSL_SDHC: 0
*** Warning - bad CRC, using default environment
EEPROM: Invalid ID (ff ff ff ff)
PCIe1: Endpoint, undetermined, regs @ 0xfe240000
PCIe1: Bus 00 - 00
PCIe2: Root Complex, x2 gen2, regs @ 0xfe250000
02:00.0 - 1957:0808 - Processor
PCIe2: Bus 01 - 02
PCIe3: disabled
PCIe4: Root Complex, x4 gen2, regs @ 0xfe270000
04:00.0 - 10ee:7022 - Memory controller
PCIe4: Bus 03 - 04
In: serial
Out: serial
Err: serial
=> pci header 4.0.0
vendor ID = 0x10ee
device ID = 0x7022
command register = 0x0007
status register = 0x0010
revision ID = 0x00
class code = 0x05 (Memory controller)
sub class code = 0x80
programming interface = 0x00
cache line = 0x08
latency time = 0x00
header type = 0x00
BIST = 0x00
base address 0 = 0xc000000c
base address 1 = 0x00001000
base address 2 = 0xe000000c
base address 3 = 0x00000000
base address 4 = 0x00000000
base address 5 = 0x00000000
cardBus CIS pointer = 0x00000000
sub system vendor ID = 0x10ee
sub system ID = 0x0007
expansion ROM base address = 0x00000000
interrupt line = 0xff
interrupt pin = 0x00
min Grant = 0x00
max Latency = 0x00
=> md fe000c00 80
fe000c00: 0000000f e8000000 81f0001b 00000000 ................
fe000c10: 0000000f f4000000 81800018 00000000 ................
fe000c20: 0000000f f6000000 83c00018 00000000 ................
fe000c30: 0000000f ffdf0000 81f0000b 00000000 ................
fe000c40: 0000000f 00000000 81d00018 00000000 ................
fe000c50: 0000000f ff800000 81f00013 00000000 ................
fe000c60: 0000000c 00000000 8000001c 00000000 ................
fe000c70: 0000000f f8000000 8000000f 00000000 ................
fe000c80: 0000000c 20000000 8010001b 00000000 .... ...........
fe000c90: 0000000f f8010000 8010000f 00000000 ................
fe000ca0: 0000000c 40000000 8030001b 00000000 ....@....0......
fe000cb0: 0000000f f8030000 8030000f 00000000 .........0......
fe000cc0: 00000000 00000000 00000000 00000000 ................
fe000cd0: 00000000 00000000 00000000 00000000 ................
fe000ce0: 00000000 00000000 00000000 00000000 ................
fe000cf0: 00000000 00000000 00000000 00000000 ................
fe000d00: 00000000 00000000 00000000 00000000 ................
fe000d10: 00000000 00000000 00000000 00000000 ................
fe000d20: 00000000 00000000 00000000 00000000 ................
fe000d30: 00000000 00000000 00000000 00000000 ................
fe000d40: 00000000 00000000 00000000 00000000 ................
fe000d50: 00000000 00000000 00000000 00000000 ................
fe000d60: 00000000 00000000 00000000 00000000 ................
fe000d70: 00000000 00000000 00000000 00000000 ................
fe000d80: 00000000 00000000 00000000 00000000 ................
fe000d90: 00000000 00000000 00000000 00000000 ................
fe000da0: 00000000 00000000 00000000 00000000 ................
fe000db0: 00000000 00000000 00000000 00000000 ................
fe000dc0: 00000000 00000000 00000000 00000000 ................
fe000dd0: 00000000 00000000 00000000 00000000 ................
fe000de0: 00000000 00000000 00000000 00000000 ................
fe000df0: 00000000 00000000 8100001f 00000000 ................
=> md fe270000 400
fe270000: 8001ff00 ffffffff 00000000 0013ffff ................
fe270010: 0400ffff 00080028 00000000 00000000 .......(........
fe270020: 00000000 00000000 000cffff 00000000 ................
fe270030: 00000000 00000000 00000000 00000000 ................
fe270040: 00000184 00000000 00000000 00000000 ................
fe270050: 00000000 00000000 00000000 00000000 ................
fe270060: 00000000 00000000 00000000 00000000 ................
fe270070: 00000000 00000000 00000000 00000000 ................
fe270080: 00000000 00000000 00000000 00000000 ................
fe270090: 00000000 00000000 00000000 00000000 ................
fe2700a0: 00000000 00000000 00000000 00000000 ................
fe2700b0: 00000000 00000000 00000000 00000000 ................
fe2700c0: 00000000 00000000 00000000 00000000 ................
fe2700d0: 00000000 00000000 00000000 00000000 ................
fe2700e0: 00000000 00000000 00000000 00000000 ................
fe2700f0: 00000000 00000000 00000000 00000000 ................
fe270100: 00000000 00000000 00000000 00000000 ................
fe270110: 00000000 00000000 00000000 00000000 ................
fe270120: 00000000 00000000 00000000 00000000 ................
fe270130: 00000000 00000000 00000000 00000000 ................
fe270140: 00000000 00000000 00000000 00000000 ................
fe270150: 00000000 00000000 00000000 00000000 ................
fe270160: 00000000 00000000 00000000 00000000 ................
fe270170: 00000000 00000000 00000000 00000000 ................
fe270180: 00000000 00000000 00000000 00000000 ................
fe270190: 00000000 00000000 00000000 00000000 ................
fe2701a0: 00000000 00000000 00000000 00000000 ................
fe2701b0: 00000000 00000000 00000000 00000000 ................
fe2701c0: 00000000 00000000 00000000 00000000 ................
fe2701d0: 00000000 00000000 00000000 00000000 ................
fe2701e0: 00000000 00000000 00000000 00000000 ................
fe2701f0: 00000000 00000000 00000000 00000000 ................
fe270200: 00000000 00000000 00000000 00000000 ................
fe270210: 00000000 00000000 00000000 00000000 ................
fe270220: 00000000 00000000 00000000 00000000 ................
fe270230: 00000000 00000000 00000000 00000000 ................
fe270240: 00000000 00000000 00000000 00000000 ................
fe270250: 00000000 00000000 00000000 00000000 ................
fe270260: 00000000 00000000 00000000 00000000 ................
fe270270: 00000000 00000000 00000000 00000000 ................
fe270280: 00000000 00000000 00000000 00000000 ................
fe270290: 00000000 00000000 00000000 00000000 ................
fe2702a0: 00000000 00000000 00000000 00000000 ................
fe2702b0: 00000000 00000000 00000000 00000000 ................
fe2702c0: 00000000 00000000 00000000 00000000 ................
fe2702d0: 00000000 00000000 00000000 00000000 ................
fe2702e0: 00000000 00000000 00000000 00000000 ................
fe2702f0: 00000000 00000000 00000000 00000000 ................
fe270300: 00000000 00000000 00000000 00000000 ................
fe270310: 00000000 00000000 00000000 00000000 ................
fe270320: 00000000 00000000 00000000 00000000 ................
fe270330: 00000000 00000000 00000000 00000000 ................
fe270340: 00000000 00000000 00000000 00000000 ................
fe270350: 00000000 00000000 00000000 00000000 ................
fe270360: 00000000 00000000 00000000 00000000 ................
fe270370: 00000000 00000000 00000000 00000000 ................
fe270380: 00000000 00000000 00000000 00000000 ................
fe270390: 00000000 00000000 00000000 00000000 ................
fe2703a0: 00000000 00000000 00000000 00000000 ................
fe2703b0: 00000000 00000000 00000000 00000000 ................
fe2703c0: 00000000 00000000 00000000 00000000 ................
fe2703d0: 00000000 00000000 00000000 00000000 ................
fe2703e0: 00000000 00000000 00000000 00000000 ................
fe2703f0: 00000000 00000000 00000000 00000000 ................
fe270400: 00000000 00000000 00000000 00000000 ................
fe270410: 00000000 00000000 00000000 00000000 ................
fe270420: 00000000 00000000 00000000 00000000 ................
fe270430: 00000000 00000000 00000000 00000000 ................
fe270440: 00000000 00000000 00000000 00000000 ................
fe270450: 00000000 00000000 00000000 00000000 ................
fe270460: 00000000 00000000 00000000 00000000 ................
fe270470: 00000000 00000000 00000000 00000000 ................
fe270480: 00000000 00000000 00000000 00000000 ................
fe270490: 00000000 00000000 00000000 00000000 ................
fe2704a0: 00000000 00000000 00000000 00000000 ................
fe2704b0: 00000000 00000000 00000000 00000000 ................
fe2704c0: 00000000 00000000 00000000 00000000 ................
fe2704d0: 00000000 00000000 00000000 00000000 ................
fe2704e0: 00000000 00000000 00000000 00000000 ................
fe2704f0: 00000000 00000000 00000000 00000000 ................
fe270500: 00000000 00000000 00000000 00000000 ................
fe270510: 00000000 00000000 00000000 00000000 ................
fe270520: 00000000 00000000 00000000 00000000 ................
fe270530: 00000000 00000000 00000000 00000000 ................
fe270540: 00000000 00000000 00000000 00000000 ................
fe270550: 00000000 00000000 00000000 00000000 ................
fe270560: 00000000 00000000 00000000 00000000 ................
fe270570: 00000000 00000000 00000000 00000000 ................
fe270580: 00000000 00000000 00000000 00000000 ................
fe270590: 00000000 00000000 00000000 00000000 ................
fe2705a0: 00000000 00000000 00000000 00000000 ................
fe2705b0: 00000000 00000000 00000000 00000000 ................
fe2705c0: 00000000 00000000 00000000 00000000 ................
fe2705d0: 00000000 00000000 00000000 00000000 ................
fe2705e0: 00000000 00000000 00000000 00000000 ................
fe2705f0: 00000000 00000000 00000000 00000000 ................
fe270600: 00000000 00000000 00000000 00000000 ................
fe270610: 00000000 00000000 00000000 00000000 ................
fe270620: 00000000 00000000 00000000 00000000 ................
fe270630: 00000000 00000000 00000000 00000000 ................
fe270640: 00000000 00000000 00000000 00000000 ................
fe270650: 00000000 00000000 00000000 00000000 ................
fe270660: 00000000 00000000 00000000 00000000 ................
fe270670: 00000000 00000000 00000000 00000000 ................
fe270680: 00000000 00000000 00000000 00000000 ................
fe270690: 00000000 00000000 00000000 00000000 ................
fe2706a0: 00000000 00000000 00000000 00000000 ................
fe2706b0: 00000000 00000000 00000000 00000000 ................
fe2706c0: 00000000 00000000 00000000 00000000 ................
fe2706d0: 00000000 00000000 00000000 00000000 ................
fe2706e0: 00000000 00000000 00000000 00000000 ................
fe2706f0: 00000000 00000000 00000000 00000000 ................
fe270700: 00000000 00000000 00000000 00000000 ................
fe270710: 00000000 00000000 00000000 00000000 ................
fe270720: 00000000 00000000 00000000 00000000 ................
fe270730: 00000000 00000000 00000000 00000000 ................
fe270740: 00000000 00000000 00000000 00000000 ................
fe270750: 00000000 00000000 00000000 00000000 ................
fe270760: 00000000 00000000 00000000 00000000 ................
fe270770: 00000000 00000000 00000000 00000000 ................
fe270780: 00000000 00000000 00000000 00000000 ................
fe270790: 00000000 00000000 00000000 00000000 ................
fe2707a0: 00000000 00000000 00000000 00000000 ................
fe2707b0: 00000000 00000000 00000000 00000000 ................
fe2707c0: 00000000 00000000 00000000 00000000 ................
fe2707d0: 00000000 00000000 00000000 00000000 ................
fe2707e0: 00000000 00000000 00000000 00000000 ................
fe2707f0: 00000000 00000000 00000000 00000000 ................
fe270800: 00000000 00000000 00000000 00000000 ................
fe270810: 00000000 00000000 00000000 00000000 ................
fe270820: 00000000 00000000 00000000 00000000 ................
fe270830: 00000000 00000000 00000000 00000000 ................
fe270840: 00000000 00000000 00000000 00000000 ................
fe270850: 00000000 00000000 00000000 00000000 ................
fe270860: 00000000 00000000 00000000 00000000 ................
fe270870: 00000000 00000000 00000000 00000000 ................
fe270880: 00000000 00000000 00000000 00000000 ................
fe270890: 00000000 00000000 00000000 00000000 ................
fe2708a0: 00000000 00000000 00000000 00000000 ................
fe2708b0: 00000000 00000000 00000000 00000000 ................
fe2708c0: 00000000 00000000 00000000 00000000 ................
fe2708d0: 00000000 00000000 00000000 00000000 ................
fe2708e0: 00000000 00000000 00000000 00000000 ................
fe2708f0: 00000000 00000000 00000000 00000000 ................
fe270900: 00000000 00000000 00000000 00000000 ................
fe270910: 00000000 00000000 00000000 00000000 ................
fe270920: 00000000 00000000 00000000 00000000 ................
fe270930: 00000000 00000000 00000000 00000000 ................
fe270940: 00000000 00000000 00000000 00000000 ................
fe270950: 00000000 00000000 00000000 00000000 ................
fe270960: 00000000 00000000 00000000 00000000 ................
fe270970: 00000000 00000000 00000000 00000000 ................
fe270980: 00000000 00000000 00000000 00000000 ................
fe270990: 00000000 00000000 00000000 00000000 ................
fe2709a0: 00000000 00000000 00000000 00000000 ................
fe2709b0: 00000000 00000000 00000000 00000000 ................
fe2709c0: 00000000 00000000 00000000 00000000 ................
fe2709d0: 00000000 00000000 00000000 00000000 ................
fe2709e0: 00000000 00000000 00000000 00000000 ................
fe2709f0: 00000000 00000000 00000000 00000000 ................
fe270a00: 00000000 00000000 00000000 00000000 ................
fe270a10: 00000000 00000000 00000000 00000000 ................
fe270a20: 00000000 00000000 00000000 00000000 ................
fe270a30: 00000000 00000000 00000000 00000000 ................
fe270a40: 00000000 00000000 00000000 00000000 ................
fe270a50: 00000000 00000000 00000000 00000000 ................
fe270a60: 00000000 00000000 00000000 00000000 ................
fe270a70: 00000000 00000000 00000000 00000000 ................
fe270a80: 00000000 00000000 00000000 00000000 ................
fe270a90: 00000000 00000000 00000000 00000000 ................
fe270aa0: 00000000 00000000 00000000 00000000 ................
fe270ab0: 00000000 00000000 00000000 00000000 ................
fe270ac0: 00000000 00000000 00000000 00000000 ................
fe270ad0: 00000000 00000000 00000000 00000000 ................
fe270ae0: 00000000 00000000 00000000 00000000 ................
fe270af0: 00000000 00000000 00000000 00000000 ................
fe270b00: 00000000 00000000 00000000 00000000 ................
fe270b10: 00000000 00000000 00000000 00000000 ................
fe270b20: 00000000 00000000 00000000 00000000 ................
fe270b30: 00000000 00000000 00000000 00000000 ................
fe270b40: 00000000 00000000 00000000 00000000 ................
fe270b50: 00000000 00000000 00000000 00000000 ................
fe270b60: 00000000 00000000 00000000 00000000 ................
fe270b70: 00000000 00000000 00000000 00000000 ................
fe270b80: 00000000 00000000 00000000 00000000 ................
fe270b90: 00000000 00000000 00000000 00000000 ................
fe270ba0: 00000000 00000000 00000000 00000000 ................
fe270bb0: 00000000 00000000 00000000 00000000 ................
fe270bc0: 00000000 00000000 00000000 00000000 ................
fe270bd0: 00000000 00000000 00000000 00000000 ................
fe270be0: 00000000 00000000 00000000 00000000 ................
fe270bf0: 00000000 00000000 02080300 00000000 ................
fe270c00: 00000000 00000000 00000000 00000000 ................
fe270c10: 80044027 00000000 00000000 00000000 ..@'............
fe270c20: 000e0000 00000000 00c40000 00000000 ................
fe270c30: 8004401b 00000000 00000000 00000000 ..@.............
fe270c40: 00000000 00000000 00ff8030 00000000 ...........0....
fe270c50: 8008800f 00000000 00000000 00000000 ................
fe270c60: 00000000 00000000 00000000 00000000 ................
fe270c70: 00000000 00000000 00000000 00000000 ................
fe270c80: 00000000 00000000 00000000 00000000 ................
fe270c90: 00044027 00000000 00000000 00000000 ..@'............
fe270ca0: 00000000 00000000 00000000 00000000 ................
fe270cb0: 00000000 00000000 00000000 00000000 ................
fe270cc0: 00000000 00000000 00000000 00000000 ................
fe270cd0: 00000000 00000000 00000000 00000000 ................
fe270ce0: 00000000 00000000 00000000 00000000 ................
fe270cf0: 20f44017 00000000 00000000 00000000 .@.............
fe270d00: 00ffe000 00000000 00000000 00000000 ................
fe270d10: 00e44017 00000000 00000000 00000000 ..@.............
fe270d20: 00000000 00000000 00000000 00000000 ................
fe270d30: 00000000 00000000 00000000 00000000 ................
fe270d40: 00000000 00000000 00000000 00000000 ................
fe270d50: 00000000 00000000 00000000 00000000 ................
fe270d60: 00000000 00000000 00000000 00000000 ................
fe270d70: 00000000 00000000 00000000 00000000 ................
fe270d80: 00000000 00000000 00000000 00000000 ................
fe270d90: 20f44027 00000000 00000000 00000000 .@'............
fe270da0: 00000000 00000000 01000000 00000000 ................
fe270db0: a0f5501f 00000000 00000000 00000000 ..P.............
fe270dc0: 00000000 00000000 00000000 00000000 ................
fe270dd0: a0f5501f 00000000 00000000 00000000 ..P.............
fe270de0: 00ffe000 00000000 00000000 00000000 ................
fe270df0: 80e44017 00000000 00000000 00000000 ..@.............
fe270e00: 80020000 00000000 00fdfeb6 00000000 ................
fe270e10: 00000000 00000000 00000000 00000000 ................
fe270e20: 80000001 00000000 00000800 00000000 ................
fe270e30: 00000000 00000000 00000000 00000000 ................
fe270e40: 00000000 00000000 00000000 00000000 ................
fe270e50: 00000000 00000000 00000000 00000000 ................
fe270e60: 00000000 00000000 00000000 00000000 ................
fe270e70: 00000000 00000000 00000000 00000000 ................
fe270e80: 00000000 00000000 00000000 00000000 ................
fe270e90: 00000000 00000000 00000000 00000000 ................
fe270ea0: 00000000 00000000 00000000 00000000 ................
fe270eb0: 00000000 00000000 00000000 00000000 ................
fe270ec0: 00000000 00000000 00000000 00000000 ................
fe270ed0: 00000000 00000000 00000000 00000000 ................
fe270ee0: 00000000 00000000 00000000 00000000 ................
fe270ef0: 00000000 00000000 00000000 00000000 ................
fe270f00: 80400084 00000000 00000000 00000000 .@..............
fe270f10: cc800000 90000044 00ff0000 00000000 .......D........
fe270f20: 00008000 00000000 00000000 00000000 ................
fe270f30: 00000000 00000000 00000000 00000000 ................
fe270f40: 00000000 00000000 00000000 00000000 ................
fe270f50: 00000000 00000000 00000000 00000000 ................
fe270f60: 00000000 00000000 00000000 00000000 ................
fe270f70: 00000000 00000000 00000000 00000000 ................
fe270f80: 00000000 00000000 00000000 00000000 ................
fe270f90: 00000000 00000000 00000000 00000000 ................
fe270fa0: 00000000 00000000 00000000 00000000 ................
fe270fb0: 00000000 00000000 00000000 00000000 ................
fe270fc0: 00000000 00000000 00000000 00000000 ................
fe270fd0: 00000000 00000000 00000000 00000000 ................
fe270fe0: 00000000 00000000 00000000 00000000 ................
fe270ff0: 00000000 00000000 00000000 00000000 ................
thanks for your help. Do you see anything wrong?
According to the provided dumps the U-Boot was able to configure BAR2 of the FPGA:
> base address 2 = 0xe000000c
in accordance with LAW:
> fe000ca0: 0000000c 40000000 8030001b 00000000
and Outbound ATMU:
> fe270c20: 000e0000 00000000 00c40000 00000000
> fe270c30: 8004401b 00000000 00000000 00000000
I.e physical address of the FPGA memory is 0xC_4000_0000.
The issue definitely is not connected with the T2080 hardware.
Please check wheter the FPGA's BAR0 is a 32-bit memory space BAR and it is needed to use a 64-bit BAR.
Which sortware is in question?
Have you tried to enumerate the FPGA using U-Boot from the Freescale/NXP SDK 1.9?
Thank very much for your answer.
-I haven not change anything in Yocto project source, neather dtb nor u-boot from SDK 1.8.
-The FPGA has a 64-bit memory space BAR. I have tried the same FPGA with 32-bit memory space BAR and work properly. It does not work when the FPGA has 64-bit memory space BAR.
I do not know where the problem is. Do I have to change the U-Boot? Do I have to make any change in the device Tree? If I have to, how can I do it?
I have not tried to enumerate the FPGA using U-boot. How can I do that?
I got from linux the following:
lspci
0001:00:00.0 PCI bridge: Freescale Semiconductor Inc Device 0830 (rev 11)
0001:01:00.0 Power PC: Freescale Semiconductor Inc Device 0808 (rev 10)
0002:00:00.0 PCI bridge: Freescale Semiconductor Inc Device 0830 (rev 11)
0002:01:00.0 Memory controller: Xilinx Corporation Device 7022
lspci -v
0002:01:00.0 Memory controller: Xilinx Corporation Device 7022
Subsystem: Xilinx Corporation Device 0007
Flags: bus master, fast devsel, latency 0
Memory at <ignored> (64-bit, prefetchable)
Memory at c40000000 (64-bit, prefetchable) [size=64K]
Capabilities: [40] Power Management version 3
Capabilities: [48] MSI: Enable- Count=1/8 Maskable- 64bit+
Capabilities: [60] Express Endpoint, MSI 00
Capabilities: [100] Device Serial Number 00-00-00-00-00-00-00-00
Kernel driver in use: pci
lspci -x
0002:01:00.0 Memory controller: Xilinx Corporation Device 7022
00: ee 10 22 70 07 00 10 00 00 00 80 05 08 00 00 00
10: 0c 00 00 c0 00 10 00 00 0c 00 00 e0 00 00 00 00
20: 00 00 00 00 00 00 00 00 00 00 00 00 ee 10 07 00
30: 00 00 00 00 40 00 00 00 00 00 00 00 ff 00 00 00
from U-boot
PCIe1: Endpoint, no link, regs @ 0xfe240000
PCIe1: Bus 00 - 00
PCIe2: Root Complex, x2 gen2, regs @ 0xfe250000
02:00.0 - 1957:0808 - Processor
PCIe2: Bus 01 - 02
PCIe3: disabled
PCIe4: Root Complex, x4 gen2, regs @ 0xfe270000
04:00.0 - 10ee:7022 - Memory controller
/pcie@ffe270000: PCICSRBAR @ 0xff000007
/pcie@ffe270000: Setup 64-bit PCI DMA window
/pcie@ffe270000: WARNING: Outbound window cfg leaves gaps in memory map. Adjusting the memory map could reduce unnecessary bounce buffering.
/pcie@ffe270000: DMA window size is 0xe0000000
EDAC PCI2: Giving out device to module 'MPC85xx_edac' controller 'mpc85xx_pci_err': DEV 'ffe270000.pcie' (INTERRUPT)
MPC85xx_edac acquired irq 23 for PCI Err
MPC85xx_edac PCI err registered
software IO TLB [mem 0x083ec000-0x0c3ec000] (64MB) mapped at [c0000000083ec000-c00000000c3ebfff]
PCI: Probing PCI hardware
fsl-pci ffe250000.pcie: PCI host bridge to bus 0001:00
pci_bus 0001:00: root bus resource [io 0x10000-0x1ffff] (bus address [0x0000-0xffff])
pci_bus 0001:00: root bus resource [mem 0xc20000000-0xc2fffffff] (bus address [0xe0000000-0xefffffff])
pci_bus 0001:00: root bus resource [bus 00-01]
pci 0001:00:00.0: ignoring class 0x0b2000 (doesn't match header type 01)
pci 0001:00:00.0: PCI bridge to [bus 01-ff]
fsl-pci ffe270000.pcie: PCI host bridge to bus 0002:00
pci_bus 0002:00: root bus resource [io 0x21000-0x30fff] (bus address [0x0000-0xffff])
pci_bus 0002:00: root bus resource [mem 0xc40000000-0xc4fffffff] (bus address [0xe0000000-0xefffffff])
pci_bus 0002:00: root bus resource [bus 00-01]
pci 0002:00:00.0: ignoring class 0x0b2000 (doesn't match header type 01)
pci 0002:00:00.0: PCI bridge to [bus 01-ff]
PCI: Cannot allocate resource region 0 of device 0002:01:00.0, will remap
pci 0001:00:00.0: PCI bridge to [bus 01]
pci 0001:00:00.0: bridge window [io 0x10000-0x1ffff]
pci 0001:00:00.0: bridge window [mem 0xc20000000-0xc2fffffff]
pci 0002:00:00.0: BAR 9: can't assign mem pref (size 0x40000000)
pci 0002:01:00.0: BAR 0: can't assign mem pref (size 0x40000000)
pci 0002:00:00.0: PCI bridge to [bus 01]
pci 0002:00:00.0: bridge window [io 0x21000-0x30fff]
pci 0002:00:00.0: bridge window [mem 0xc40000000-0xc4fffffff]
pci_bus 0002:00: Some PCI device resources are unassigned, try booting with pci=realloc
Do you need more information? How can I get the information that you need?thanks very much
1) Please provide output of the U-Boot command "pci header 4.0.0".
There is not device in 4.0.0 however vendor and device ID show up in 3.0.0. You can see:
=> pci header 3.0.0
vendor ID = 0x10ee
device ID = 0x7022
command register = 0x0007
status register = 0x0010
revision ID = 0x00
class code = 0x05 (Memory controller)
sub class code = 0x80
programming interface = 0x00
cache line = 0x08
latency time = 0x00
header type = 0x00
BIST = 0x00
base address 0 = 0xc000000c
base address 1 = 0x00001000
base address 2 = 0xe000000c
base address 3 = 0x00000000
base address 4 = 0x00000000
base address 5 = 0x00000000
cardBus CIS pointer = 0x00000000
sub system vendor ID = 0x10ee
sub system ID = 0x0007
expansion ROM base address = 0x00000000
interrupt line = 0xff
interrupt pin = 0x00
min Grant = 0x00
max Latency = 0x00
2) Is there a Reference Manual or User Guide for the FPGA PCIe implementation?
The PCI device FW is correct. I have tried in another system and works. I think the problem is the U-Boot or the device tree in my T2080RDB. The U-boot look like it does not realize that it a pci device working with 64 bits memories. You can see. There are 6 BAR. In a 64bit PCI device should be only 3 BAR.
Any solution?
Hi udefor,
I have tried the new version SDK 1.9. However, the problem persists.Any other solution? should I change anything in uboot, device tree or CCSR?
=> pci header 3.0.0
vendor ID = 0x10ee
device ID = 0x7022
command register = 0x0007
status register = 0x0010
revision ID = 0x00
class code = 0x05 (Memory controller)
sub class code = 0x80
programming interface = 0x00
cache line = 0x08
latency time = 0x00
header type = 0x00
BIST = 0x00
base address 0 = 0xc000000c
base address 1 = 0x00001000
base address 2 = 0xe000000c
base address 3 = 0x00000000
base address 4 = 0x00000000
base address 5 = 0x00000000
cardBus CIS pointer = 0x00000000
sub system vendor ID = 0x10ee
sub system ID = 0x0007
expansion ROM base address = 0x00000000
interrupt line = 0xff
interrupt pin = 0x00
min Grant = 0x00
max Latency = 0x00