@NXP is not going to maintain the support for u-boot?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

@NXP is not going to maintain the support for u-boot?

1,850件の閲覧回数
robertoinnocent
Contributor III

As NXP Devkit based on T1,T2,T4 CPU boot with u-boot,

and now u-boot is going dropping support to PPC (and m68k) its a big problem? isn't it?

"u-boot drop support for PPC and m68k boards because these boards have not been converted to CONFIG_DM_PCI configuration by the deadline."

In the u-boot mailing list u-boot they wrote:
The platform can come back if someone is going to be actively
maintaining the support.  No one had been doing that, so I'm not sure
what hidden breakage existed underneath the technical debt.
 
@nxp is not going to maintain the support for u-boot?
 
There are bootloader alternative? open firmware, coreboot, grub ?
 
ラベル(3)
0 件の賞賛
4 返答(返信)

1,641件の閲覧回数
robertoinnocent
Contributor III

So NXP contribute to mainline u-boot or you have a separated fork ?

I have find this repository that is related to MXP QoriQ processors https://source.codeaurora.org/external/qoriq/qoriq-components/u-boot/

Or is better to reference to the main line u-boot? https://github.com/u-boot/u-boot

Thanks!

 

0 件の賞賛

1,839件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

NXP still maintains the support for u-boot on T1,T2 and T4 platform.

0 件の賞賛

1,821件の閲覧回数
robertoinnocent
Contributor III

So NXP will continue to contribute to u-boot in terms that new release of u-boot still works with powerpc?

0 件の賞賛

1,812件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Yes

0 件の賞賛