Multiple Ethernet Port in u-boot

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multiple Ethernet Port in u-boot

4,542 Views
vinothkumars
Senior Contributor IV

Dear NXP,

 

I am working on T4240RDB-64B machine.

I am using 8 Ethernet Port and able to ping single port at the time by using ethact command.

I want to configure multiple Ethernet Port support. And the u-boot version is 2016

I am following this thread but, I not get anything from that.

Can u-boot support more than one ethernet port?

And I checked the u-boot code and by default u-boot code will support the Single Port only.

I needs to know, is there any possible to make multi port support ?

Thanks & Regards,

VinothS,

Regards,
Vinothkumar Sekar
Labels (1)
0 Kudos
Reply
6 Replies

4,311 Views
bpe
NXP Employee
NXP Employee

As it was explained above, both u-Boot and Linux support multiple network
interfaces, however, the approach is significantly different. Linux
has a full-feature IP network stack which allows a very wide range
of network related operations to be done. You did not specify
what exactly you want to do, thus the answer is, unless you want to
do something fundamentally incorrect from IP networking standpoint,
there should be a way to do that under Linux.


Have a great day,
Platon

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

4,311 Views
vinothkumars
Senior Contributor IV

Thank you Bpe.

Regards,

VinothS,

Regards,
Vinothkumar Sekar
0 Kudos
Reply

4,311 Views
bpe
NXP Employee
NXP Employee

u-Boot is only a bootloader. You should not expect a full-feature
IP stack functionality from it. u-Boot does support multiple Ethernet
interfaces, but you can use them one at a time. If you connect more than
one Ethernet link to a u-Boot-controlled box, and all links are active,
you have to specify which link to use by assigning a value to  "ethact"
environment variable. If anything above that is desired, e.g. membership
in more than one IP subnet, packet forwarding, advanced diagnostics,
the suggestion is to boot Linux or another OS with a full IP stack
implementation.


Have a great day,
Platon

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

4,311 Views
vinothkumars
Senior Contributor IV

Thank you Bpe for your reply.

Is it possible in linux?

Regards,

VinothS,

Regards,
Vinothkumar Sekar
0 Kudos
Reply

4,311 Views
bpe
NXP Employee
NXP Employee

Not sure what exactly feature you are asking about. If you are not familiar with LInux networking, study this.

Hope this helps

Platon

0 Kudos
Reply

4,311 Views
vinothkumars
Senior Contributor IV

I am asking about Ethernet Multi Port in Linux.

Regards,

VinothS,

Regards,
Vinothkumar Sekar
0 Kudos
Reply