Missing FMAN QMI registers from Documentation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Missing FMAN QMI registers from Documentation

559 Views
raymondhaas
Contributor I

I am trying to understand how the FMAN Ethernet code works in u-boot for the T1024 processor.  I am using the following documentation: QorIQ T1024 Data Path Acceleration Architecture (DPAA) Reference Manual, rev. 0.  In u-boot they are referencing registers that do not appear in the documentation.  Specifically in the FMAN QMI memory block, u-boot is updating FMQM_IEN (0x418) and FMQM_IE (0x414).  I have looked at most of the code and noticed that sometimes bit definitions have changed within some registers.

The document I am using is the latest.  I was wondering if those register actually exist, or is u-boot not up to date with the register definitions?

Thank you for your help.

Labels (1)
0 Kudos
1 Reply

440 Views
ufedor
NXP Employee
NXP Employee

The registers in question are for internal use and debug purposes.

These registers were present in the early revision of the DPAARM:

https://www.nxp.com/webapp/Download?colCode=DPAARM&location=null&fsrch=1&sr=4&pageNum=1&Parent_nodeI... 

0 Kudos