Marvel Ethernet Switch connection issue with T1022 Processor

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Marvel Ethernet Switch connection issue with T1022 Processor

Jump to solution
1,036 Views
hemwant
Contributor IV

We are having T1022 processor customized board , the SERDES configuration used in the RCW is 0x40.  The EC1 is connected to ethernet marvel switch (88E6320) port 5 with RGMII interface. Now we have initialised marvel switch port 5 with following configuration - speed 1G , full duplex autoneg off with forced link up.  The processor is able to receive ICMP packets from switch but is not sending the ICMP reply. All delay combination of rgmii have been tried in device tree as well as in switch.

I am attaching device tree which i am using for the above purpose.

Labels (1)
0 Kudos
1 Solution
987 Views
hemwant
Contributor IV

In my case , by mistake one bridge was working on the above ethernet interface. After removing the above bridge configuration the issue was solved.

View solution in original post

0 Kudos
1 Reply
988 Views
hemwant
Contributor IV

In my case , by mistake one bridge was working on the above ethernet interface. After removing the above bridge configuration the issue was solved.

0 Kudos