We are having T1022 processor customized board , the SERDES configuration used in the RCW is 0x40. The EC1 is connected to ethernet marvel switch (88E6320) port 5 with RGMII interface. Now we have initialised marvel switch port 5 with following configuration - speed 1G , full duplex autoneg off with forced link up. The processor is able to receive ICMP packets from switch but is not sending the ICMP reply. All delay combination of rgmii have been tried in device tree as well as in switch.
I am attaching device tree which i am using for the above purpose.
解決済! 解決策の投稿を見る。
In my case , by mistake one bridge was working on the above ethernet interface. After removing the above bridge configuration the issue was solved.
In my case , by mistake one bridge was working on the above ethernet interface. After removing the above bridge configuration the issue was solved.