Hello NXP
How to build LSDK 19.09 with RT version 4.14.122 steps currently its using the version 4.14.53 when it try to give build for LSDK.
regards,
ranga
Please refer to the following procedure
$ flex-builder -c linux:linux:LSDK-19.09-V4.14 -a arm64
Then replace packages/linux/linux/ with source code of Linux Kernel 4.14.122.
Run the following command to build Linux 4.14.122.
$ flex-builder -c linux -a arm64
Get Kernel image in build/linux/linux/arm64/LS/Image