Issue booting 64bit elf file from uboot on t2080 rdb

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Issue booting 64bit elf file from uboot on t2080 rdb

1,954 Views
m2sawyer
Contributor I

Questions:

1) Is uboot capable of booting a 64bit elf file on the T2080RDB?

2) Do some of the configuration options need to be changed to successfully load a 64bit elf file on uboot?

3) Is there a version of uboot I can flash on the target to load a 64bit elf binary?

Details:

I’m trying to boot a 64bit elf file from uboot on the T2080RDB-PC rev.C board, the version of uboot I am using is:

=> version

 

U-Boot 2016.012.0+ga9b437f (May 15 2016 - 10:38:22 +0800)

powerpc-fslmllib32-linux-gcc (GCC) 4.9.2

GNU ld (GNU Binutils) 2.25

 

And the output of readelf on the header of the file I am trying to load looks like so:

ELF Header:

  Magic:   7f 45 4c 46 02 02 01 00 00 00 00 00 00 00 00 00

  Class:                             ELF64

  Data:                              2's complement, big endian

  Version:                           1 (current)

  OS/ABI:                            UNIX - System V

  ABI Version:                       0

  Type:                              EXEC (Executable file)

  Machine:                           PowerPC64

  Version:                           0x1

  Entry point address:               0x43a00

  Start of program headers:          64 (bytes into file)

  Start of section headers:          748560 (bytes into file)

  Flags:                             0x1

  Size of this header:               64 (bytes)

  Size of program headers:           56 (bytes)

  Number of program headers:         49

 Size of section headers:           64 (bytes)

  Number of section headers:         95

  Section header string table index: 94

 

When I try to boot the application (using tftpboot and then bootelf) I get output like below:

=> tftpboot HelloWorld

Using FM1@DTSEC3 device

TFTP from server 192.168.6.120; our IP address is 192.168.6.230

Filename 'HelloWorld'.

Load address: 0x1000000

Loading: #################################################################

         #################################################################

         ##################

         3.2 MiB/s

done

Bytes transferred = 754640 (b83d0 hex)

=> bootelf

## Starting application at 0x00000000 ...

Bad trap at PC: ffff98e8, SR: 16024900, vector=e00

NIP: FFFF98E8 XER: 00000000 LR: 7FEF0B6C REGS: 7faedbe0 TRAP: 0e00 DAR: 00000000

MSR: 16024900 EE: 0 PR: 1 FP: 0 ME: 0 IR/DR: 00

 

GPR00: 7FF02040 7FAEDCD0 7FAEDEF8 00000000 7FAF4D24 7FAEDB9B 00000020 7FAEDB9C

GPR08: FFFFFFFE 00000020 00000020 7FAEDCD0 44022082 80000000 7FF5FA48 7FAF4D20

GPR16: 7FF5FA38 0000000A 7FAF4D10 00000000 7FAF4D40 00000000 00000000 FFFF98E8

GPR24: 00000000 7FFB029C 00000001 00000000 7FAF4D24 00000000 7FF745C0 00000001

Call backtrace:

7FF02040 7FF1D060 7FEFDDDC 7FEFE59C 7FEFE64C 7FF1BA4C 7FEFBE9C

7FEFEED8 7FF4DCEC 7FEFF2E4 7FEF0F50

Exception in kernel pc ffff98e8 signal 0

 

 

It looks like it trying to start the application at 0x00000000, which really doesn’t seem correct when the start address from the elf header is 0x43a00.

Is uboot capable of booting a 64bit elf file?

Do some of the configuration options need to be changed to successfully load a 64bit elf file on uboot?

Is there a version of uboot I can flash on the target to load a 64bit elf binary?

Any help would be appreciated. 

Thanks,

t2080rdb‌ 

64-bit‌

elf‌

uboot;‌

t2080 uboot‌

Labels (1)
0 Kudos
Reply
1 Reply

1,630 Views
Pavel
NXP Employee
NXP Employee

U-boot for QorIQ is 32-bit software.

See the /cmd/elf.c in u-boot source folder.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply