Is there documentation on the E5500/T1042 boot process?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is there documentation on the E5500/T1042 boot process?

1,155件の閲覧回数
plat
Contributor I

I am going to replace U-Boot with my own bootloader. However, I can't seem to find much information on the boot process. The E5500 manual, in chapter 11, does provide a some stuff, but I was wondering if there's a document similar to the SMP Boot Process for Dual E500 Cores?

ラベル(1)
0 件の賞賛
返信
1 返信

911件の閲覧回数
ufedor
NXP Employee
NXP Employee

The processor power-on initialization sequence is complicated and there is no document containing detailed description of all steps.

Even if there is an intention to replace U-Boot with a proprietary boot loader, it is recommended to refer to the U-Boot sources included into the Linux SDK for a specific platform.

The following presentations also could be useful:

http://www.nxp.com/files/training_pdf/WBNR_FTF10_NET_F0683.pdf 

http://www.nxp.com/files/training_pdf/FTF/2012/americas/WBNR_FTF12_NET_F0180.pdf?lang_cd=en 

0 件の賞賛
返信