Is there a way to choose different processor clock rates on the T4240RDB board?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is there a way to choose different processor clock rates on the T4240RDB board?

Jump to solution
1,523 Views
nickcaruso
Contributor III

That's it, that's the question:  Is there a way to choose different processor clock rates on the T4240RDB board, either by setting options in the uboot shell, or by recompiling uboot, or ... ?

I tried to search the documentation but I couldn't find the answer.

Thanks for your help!

Labels (1)
1 Solution
1,358 Views
ufedor
NXP Employee
NXP Employee

Of course it is possible using modified RCW.

The RCW is described in the T4240 Reference Manual, 4.6.4.1 RCW Field Definitions:

https://www.nxp.com/webapp/Download?colCode=T4240RM

Current RCW is printed by U-Boot.

It could be imported and modified using the PBL Tool from the QorIQ Configuration and Validation Suite which is bundled with CodeWarrior evaluation version available at:

CodeWarrior Dev Tools for Power Architecture|NXP

The RCW programming is explained in the Linux SDK Documentation:

Submit Form

View solution in original post

1 Reply
1,359 Views
ufedor
NXP Employee
NXP Employee

Of course it is possible using modified RCW.

The RCW is described in the T4240 Reference Manual, 4.6.4.1 RCW Field Definitions:

https://www.nxp.com/webapp/Download?colCode=T4240RM

Current RCW is printed by U-Boot.

It could be imported and modified using the PBL Tool from the QorIQ Configuration and Validation Suite which is bundled with CodeWarrior evaluation version available at:

CodeWarrior Dev Tools for Power Architecture|NXP

The RCW programming is explained in the Linux SDK Documentation:

Submit Form