Is T2080 Supported in current Linux Kernels?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Is T2080 Supported in current Linux Kernels?

2,905 次查看
vladimirboroda
Contributor II

Hi,

I am looking to build linux-qoriq kernel 4.9 for our T2080-based custom board.  I was planning on using the Yocto recipes for t2080rdb as the base, but it appears that the 4.9 kernels do not carry corenet64_fmanv3h_smp_defconfig any more. 

When I copied it from Freescale SDK 2.0, it seemed to be incompatible with the newer linux-qoriq 4.9 kernel.  The "Fman Support" in Device Drivers → Network device support → Ethernet driver support can be enabled, but "Frame Manager support" selection leads to an empty screen.   In arch/powerpc/configs there is not any obvious t2080rdb configuration.

Is there a known working 4.9 kernel config for t2080rdb?  Is linux-qoriq even the right kernel variant to support T2080 and e6500 cores?

Thanks!

标签 (1)
0 项奖励
回复
4 回复数

2,127 次查看
liguofa
Contributor III

ufedorkhumphriMandar

I also encountered the same problem. When I compiled the kernel, I wanted to find a similar configuration file for T2080rdb board,So could enerybody help me.Thanks.

0 项奖励
回复

2,127 次查看
jakemoroni
Contributor II

Hello,

I was able to build and run the latest mainline kernel (4.16-rc1) on the T2080.

You want to use "corenet64_smp_defconfig". Even though that file doesn't actually exist under arch/powerpc/configs, if you look in the arch/powerpc/Makefile, you'll see that the "corenet64_smp_defconfig" target pulls in a bunch of config file fragments to generate the final config file.

I also used the fsl/t2080rdb device tree in the mainline kernel without issues.

- Jake Moroni

0 项奖励
回复

2,127 次查看
vidyasagar
Contributor III

Dear Moroni,

I have downloaded linux kernel (linux-fslc-4.19.x-fslc) from freescale github website, want to port in T2080RDB board similar as SDK2.0 (linux kernel4.1), please help me know the steps to follow in cross compilation and porting in T2080RDB board successfully.

I have extracted SDK2.0 kernel and toolchain  from yocto.

Thanks & Regards,

Amit

0 项奖励
回复

2,127 次查看
vidyasagar
Contributor III

Waiting for reply.

0 项奖励
回复