Hello,
I am using T1042 processor for my board. I have to use two SATA interfaces, all four PCI express interfaces and two 1G Ethernet Interface. My question is that is there any possibility that I can use them without using SERDES ? If I had to use SERDES, then which channel for which interface and how ?
Thanks in advance.
Regards,
Ather
The SerDes is used for each high-speed serial interface.
> which channel for which interface and how ?
Please refer to the QorIQ T1040 Reference Manual, Chapter 31 SerDes Module, Figure 31-1. Supported SerDes Options.