If there is a possible to run docker or other container on yocto Linux?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

If there is a possible to run docker or other container on yocto Linux?

808 次查看
eric7
Contributor I

Due to business needs, I have to isolate applications running in yocto Linux. I can think of ways to use containers, but I tried to install docker in yocto Linux without success. I am using a T4240 processor and I don’t know if there are any successful installation cases. I'd love some advice on installing the container.

0 项奖励
回复
1 回复

782 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Please download document QORIQ-SDK-2.0-IC-REV0.pdf from https://support.nxp.com/s/case/5002p00002x1B5EAAU/community-if-there-is-a-possible-to-run-docker-or-...

Then refer to the section "11.5 Docker Containers".

0 项奖励
回复