I want to debug linux application for T1024 for my custom board using on Codewarrior 10.5.0. .... My PC is not connected to internet. How do i get example linux project with toolchain. I also want to debug example project.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

I want to debug linux application for T1024 for my custom board using on Codewarrior 10.5.0. .... My PC is not connected to internet. How do i get example linux project with toolchain. I also want to debug example project.

1,200 次查看
abhishekborana
Contributor II

Codewarrior 

0 项奖励
回复
1 回复

1,142 次查看
Pavel
NXP Employee
NXP Employee

Look at attached file. It is part of the Targeting_PA_Processors.pdf file. This file is available in CodeWarrior 10.5.1 folder.

Have a great day,
Pavel Chubakov

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复