How to receive VLAN tagged packets without filtering in QorIQ T1024

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to receive VLAN tagged packets without filtering in QorIQ T1024

1,220 Views
veerendranathj
Contributor III

Hi,

I am using T1024 ethernet interface in Indepedent mode. I want to receive all frames through a port if destination MAC address matches irrespective of VLAN Tag. How can we achieve this functionality? 

Regards,

Veeru

Labels (1)
0 Kudos
Reply
1 Reply

1,108 Views
bpe
NXP Employee
NXP Employee

In independent mode neither address recognition, nor any header manipulation is possible. You always receive all frames heard on the wire, with all fields past preamble intact. Refer to T1024DPAARM, Section 5.13.15


Have a great day,
Platon

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply